Skip to main content
memorylost
Visitor II
December 16, 2020
Question

STM32CubeIDE project with H745 processor

Hi all,

I am testing H745 processor on Nucleo-H745ZI-Q board and STM32CubeIDE 1.5.0 .

I started from a demo project found in Cube library, which handles both CM7 and CM4 cores.

The IDE correctly creates one HEX file for CM4 and another HEX file for CM7, then creates a single HEX file which hopefully contains both.

It is not clear to me where are the project config options which are creating the final HEX file (CM4+CM7) : is there someone who can give me a hint for this ?

The IDE is working correctly, but I am not so "comfortable" in missing these configs.

Thanks,

regards && best wishes for Christmas and new year to all !

Lucio

This topic has been closed for replies.