Skip to main content
Andrew Neil
Super User
March 1, 2024
Question

STM32CubeIDE opens on non-present screen.

Win 11 Laptop with external (large) monitor.

When the laptop is then used without the external monitor, apps should open on the internal one.

Most do; STM32CubeIDE (v1.13.0) doesn't - it still positions itself as it the non-connected screen were still there.


Addendum

If you get stuck in this situation, the IDE window can be retrieved by:

  1. Give the IDE window focus (eg, Alt+TAB to it)
  2. Press Alt+Spacebar.
    The window control menu will appear at the edge of the real screen:
    AndrewNeil_0-1709311291831.png

     

  3. Select 'Move'.
    The cursor keys will now move the IDE window - use them to move it onto the real screen.
    This topic has been closed for replies.