Skip to main content
Associate
Dec 18, 2024 4:43 PM UTC
Question

STM32CubeIDE on MacBook (M3 Max) won't recognize NUCLEO-F446RE

TL;DR - My setup works when I use a Windows laptop, but fails when I use a MacBook Pro (M3 Max).  I am looking for help on using my MacBook Pro (M3 Max) to program my Nucleo board.

This is my first time trying to program / debug such a board.  I wrote a very simple C program to turn on the green LED (LD2) on my board:  https://github.com/rajesh-gopalan/stm32-nucleo-f446re/blob/main/0_led_toggle_addr.c

My focus is on the following basic hardware <> software setup (not the actual program content):

Host Device  - 16-inch MacBook Pro 2023, with M3 Max processor

Board             - STM32 NUCLEO-F446RE

IDE                 - STM32CubeIDE

                         Version: 1.17.0

                         Build: 23558_20241125_2245 (UTC)

Connectivity   - USB-C (host side) to Mini-B (board side) cable

As soon as I connect the cable between the board and the MacBook, the red LED (LD1) starts blinking, maybe twice a second and the other red LED (LD3) is also blinking, but its output is very feeble.  I am able to successfully build the code.  But, when I run main, the IDE indicates the following error: No ST-Link detected!  Please connect ST-LINK and restart the debug session.

 

Based on what I have been reading upon, and from recommendation in an MOOC education forum (Udemy), I took the following steps, to see if that rectifies the issue:

1. I installed HomeBrew:

    $prompt> /bin/bash -c "$(curl -fsSL https://raw.githubusercontent.com/Homebrew/install/HEAD/install.sh)"

2. I updated Rosetta:

    $prompt> softwareupdate --install-rosetta

    Rosetta 2 was installed on my MacBook Pro (with M3 Max Apple silicon)

3. I restarted my MacBook (and accordingly my Chrome Browser)

4. I installed STM32CubeIDE for MacOS and the ST-Link driver as per instructions provided in the website: https://www.st.com/en/development-tools/stm32cubeide.html

5. I used sudo to start CubeIDE:

    $prompt> sudo /Applications/STM32CubeIDE.app/Contents/MacOS/STM32CubeIDE

Though I am able to successfully build (as before), I keep getting the same error when I try to run: No ST-Link detected! Please connect ST-LINK and restart the debug session.

 

To ensure it is not a board / cable issue, I used a Windows laptop to successfully build and run my program, i.e. I was able to turn on the green LED (LD2) on my board.  But, I am unable to replicate my success on my MacBook Pro (M3 Max).  I am looking for help on using my MacBook Pro (M3 Max) to program my Nucleo board.  I am resisting a potential solve of using emulation (Windows in Mac using Parallels or Fusion Pro) to overcome this issue.

I am beginning to think my host machine is not supported by STMicro: 16-inch MacBook Pro 2023 with Apple Silicon (M3 Max, based on aarm64 architecture).  The STM32CubeIDE's install file name (en.st-stm32cubeide_1.17.0_23558_20241125_2245_x86_64) seems to indicate that it supports processors that use x86_64 architecture, and may not support processors that use aarm64 architecture.  Additionally, based on the naming convention of the ST-Link driver, it seems to support x86_64 architecture as well.

 

I appreciate the support here!

 

This topic has been closed for replies.

2 replies

Associate
Dec 18, 2024 9:54 PM UTC

If anyone here has successfully made their board work with the STM32CubeIDE running on a MacBook Pro with Apple silicon (M1, M2, M3, etc.), please let me know.  Was that achieved using Parallels Desktop / UTM to load either Linux or Windows on the MacBook?

Alternately, if the recommendation from this community is to move to a machine using Intel/AMD 64-bit processors, given STM32CubeIDE works on x86_64 architecture, I'm happy to tag that route and let this one RIP.

Associate
Jul 6, 2025 3:55 AM UTC

Hi raj_gopalan, 

Did you ever find success?