Skip to main content
angelosn
Associate
Jul 22, 2025 4:01 PM UTC
Question

STM32CubeIDE on Linux (Wayland, 4K HiDPI) – Blurry UI with X11, but CubeMX fails under Wayland

Hello STM community,

I'm experiencing a UI/UX issue with STM32CubeIDE on my Linux system and would appreciate any insight or workarounds.

My setup:

  • Distro: Arch Linux

  • KDE Plasma: 6.4.3

  • KDE Frameworks: 6.16.0

  • Qt Version: 6.9.1

  • Kernel: 6.12.39-1-lts (64-bit)

  • Graphics Platform: Wayland

  • Monitor: 4K with 150% scaling

  • CPU: AMD Ryzen 7 3800X

  • GPU: AMD Radeon RX 6600

  • Memory: 16 GiB

  • Motherboard: Gigabyte B450 AORUS PRO

I installed STM32CubeIDE 1.19.0 using the official generic Linux installer.

To improve compatibility, I’m using a launcher script (stm32cubeide_wayland) like this:

 

#!/bin/bash
basedir=$(dirname "$BASH_SOURCE")
export GDK_BACKEND=x11 
export WEBKIT_DISABLE_COMPOSITING_MODE=1
"$basedir"/stm32cubeide "$@"
 

This runs CubeIDE under X11, which allows STM32 project creation (CubeMX launches correctly), but the interface is blurry and not crisp on my HiDPI 4K screen.

blurry.png

If I instead use:

export GDK_BACKEND=wayland

...the UI becomes sharp and scales properly (as expected), but CubeMX fails to launch when trying to create a new project (no MCU or board selection dialog ever appears).

4k.png

 

My temporary workaround:

  1. Launch with X11 to create a project and edit the .ioc file..

  2. Close STM32CubeIDE.

  3. Re-launch with Wayland to enjoy crisp UI.


My questions:

  • Is this a known issue on Wayland in general, or specific to Arch Linux?

  • Is there any official fix or workaround for HiDPI support that doesn't break CubeMX functionality?

  • Does STM plan to offer native Wayland support or improved Qt scaling in the future?

Thanks in advance to anyone who has suggestions or experience with this setup!

 

This topic has been closed for replies.

1 reply

TDK
Jul 22, 2025 8:16 PM UTC

This is a QT issue, not something ST-specific. STM32CubeIDE is just a re-skinned Eclipse. Look for solutions on the web for x11 + eclipse.

I recommend using the standalone STM32CubeMX to generate projects. It is more responsive and seems to solve your issues.

"If you feel a post has answered your question, please click ""Accept as Solution""."