Skip to main content
Fabien B
Associate III
May 7, 2019 1:20 PM UTC
Solved

STM32CubeIDE NSIS Error during installation

Hello,

I downloaded STM32CubeIDE v1.0.0 and tried to install it on my Windows 7 computer.

Unfortunatly I have a NSIS Error "Error launching installer". I tried to download again the file, tried on another windows 7 PC but I still have this issue.

Someone know how to solve this issue?

Thanks and best regards

Fabien

This topic has been closed for replies.
BKani.1
BKani.1Best answer
Visitor II
Jan 12, 2020 1:08 PM UTC

Same here, in Jan 2020 on Win10 64bit;

  1. Copied unzipped directory to c:\
  2. Shortened its name to "en.st-stm32cubeide_1.2.0"
  3. Shortened the exe name to "st-stm32cubeide.exe"
  4. Installer started

24 replies

SBybe
Associate II
May 7, 2019 5:43 PM UTC

Hello! Windows 10 also has a startup problem!

Markus GIRDLAND
ST Employee
May 8, 2019 3:09 PM UTC

As a first step please make an md5sum check using the following MD5:

c1004055082e06392ea358ed796060c8

As a second step given that the first step is OK. Please check your anti-virus software log files to make sure it doesn't interfere with the launching of the installer. Please share your findings with us!

Fabien B
Fabien BAuthor
Associate III
May 9, 2019 7:23 AM UTC

Thanks for your answer but unfortunately installation still fail.

I checked the MD5 of the .exe file and it match.

I disabled my anti-virus software (Microsoft Security Essentials) but I still have the NSIS error during installation.

Markus GIRDLAND
ST Employee
May 13, 2019 11:12 AM UTC

Are you launching from a USB stick or something similar? Do the two different PCs have the same setup? With network and anti-virus software? Are the computers 32 or 64-bit?

I've tried reproducing the error on a few of my windows computers that are on different networks with different setups but no NSIS error so far. Any specific tips to help in how I can reproduce would help a lot!

SSeli.1
Visitor II
Aug 9, 2020 3:54 PM UTC

Thank you so mach!

I have a Windows 10 Pro 64-bit and I have the same problems with istallation (NSIS Error). I'm not check MD5 but for unzipping I used WinRar.

I could fix the issue after remove st-stm32cubeide_1.4.0_7511_20200720_0928_x86_64.exe in root drive C:

All started without an error!

Fabien B
Fabien BAuthor
Associate III
May 14, 2019 12:04 PM UTC

The software is on my hard drive.

Please find a summary of my tests:

  • I tried on a computers with Windows 7 SP1 Pro 64 bits, with Microsoft Security Essentials antivirus software and same network. NSIS Error.
  • I tried on a computers with Windows 7 SP1 Pro 64 bits, Microsoft Security Essentials antivirus software disable and same network. NSIS Error.
  • I tried on a computer with Windows 7 SP1 Pro 32 bits, without antivirus software and same network. NSIS Error.
  • I tried on on a computer with Windows 10 Pro 64 bits, with Avira antivirus software and same network. Installation work fine.

I also discover that if I unzip the file with windows embedded zip, the MD5 match with the one you provided to me. But, if I unzipped it with 7-zip software the MD5 doesn't match.

So I used always the file with the correct MD5 for all these tests.

Markus GIRDLAND
ST Employee
May 16, 2019 9:37 AM UTC

This is very unusual and I can't seem to reproduce it.

The fact that the Windows 7 SP1 Pro 32 bits isn't working isn't a huge deal since we only support 64 bit installers. However, you should receive a dialogue explaining that instead of an NSIS error.

I tried using the installer with Windows 7 SP1 Pro 64 bit here in the office, both with and without antivirus active, and it worked both times.

Does the path to the installer contain any non-ascii characters?

Can you place the installer right in C:/st-stm32cubeide_1.0.0_2872_20190423-2022_x86_64.exe and see if it makes a difference?

Dlouhan
Visitor II
Jun 13, 2020 9:40 AM UTC

I placed the installer in f:\pom\st-stm32cubeide_1.3.0_5720_20200220_1053_x86_64.exe from long path with non-ascii characters.

An installer ran correctly on Windows 7 SP1 - 64 bit Czech with Avast antivirus.

Thank's for good tips

Fabien B
Fabien BAuthor
Associate III
May 16, 2019 10:19 AM UTC

Thanks a lot for your help, all is working well.

Your idea was correct, the issue came from the path. In my case it was D:\Téléchargement\STM32CubeIDE

About Windows 7 32bit, the issue was an NSIS corruption file. The corruption came during unzip process. With a good .exe file, I have the correct dialogue box.

Do you have an idea about corrupted file when I used 7-zip software?

YLiu.523
Visitor II
Oct 28, 2019 6:56 AM UTC

yes, i meet the same thing. While unzip the software by 7-zip, the "NSIS ERROR" occured,

but use the WINDOWS default unzip software, i could run the install progress.

LibreServo
Visitor II
Jun 26, 2019 11:21 PM UTC

2019 and STILL with problems with accented vowels!!?? Really??

I had the same issue, and of course the installer said nothing in order to get a clue... pitiful >:(

Explorer
Apr 19, 2025 3:31 PM UTC

Fun fact: 2025 and STILL with problems with accented vowels, I has having this NSIS Error for a while before noticing the username in my brother's PC had an accent and a space.

I ended up creating a whole new profile just in case

Pawka
Visitor II
Aug 2, 2019 1:47 PM UTC

I ran into this too, and I found a solution like this:

1. Reduced the name of the folder and file to stm32cubeide_1.0.2

2. Moved the folder to the root of drive D, before it was in a folder with a name in Russian.

3. Disable 360 Total Security.

4. I use it!

Win10 Pro x64

CMach.1
Visitor II
Apr 3, 2020 12:59 AM UTC

Thank you. It work for my case.

Win 8 x64

BKani.1
BKani.1Best answer
Visitor II
Jan 12, 2020 1:08 PM UTC

Same here, in Jan 2020 on Win10 64bit;

  1. Copied unzipped directory to c:\
  2. Shortened its name to "en.st-stm32cubeide_1.2.0"
  3. Shortened the exe name to "st-stm32cubeide.exe"
  4. Installer started
Explorer
Jun 10, 2025 7:22 PM UTC

Thank you! This solution helped me

 

AZayt.1
Visitor II
Feb 11, 2020 8:49 PM UTC

Папки �? ру�?�?кими буквами мешали. Спа�?ибо, Павел.

PIvan.4
Visitor II
Apr 30, 2020 8:47 AM UTC

I had the same problem. I solve it. 2 issues:

1) Path name should be only latin symbols (no cyrillic or other characters).

2) You can just unpack zip archive with 7zip software, open the install application with 7zip extract and extract "STM32CubeIDE" directory to any path, then launch stm32cubeide.exe as portable app.