Skip to main content
DRega.1
Associate III
July 22, 2023
Question

STM32CubeIDE Multi-Threaded support

The STM32CubeIDE does not always correctly generate/regenerate the Multi-Threaded support code and ThreadSafe folder.

I noticed this when converting an existing project to use FreeRTOS. After experimenting, it seems that if the project contains virtual folders to linked resources, the ThreadSafe folder will not be generated. If the virtual folders are removed, such that the ThreadSafe folder is generated, it will not be modified if the selected strategy is changed once the virtual folders are reinstated.

    This topic has been closed for replies.

    1 reply

    Piranha
    Principal III
    July 23, 2023

    And even better question for ST is why that "ThreadSafe" folder with it's files is available only for CubeMX. Why isn't it available as a normal software component in firmware packages and GitHub in the "Utilities" directory?