Skip to main content
CharlieMangold
Senior
May 31, 2023
Question

STM32CubeIDE locks the Workspace location. Best method to modify the Workspace location so the code base is completely portable except for the compiler/linker.

  • May 31, 2023
  • 4 replies
  • 6627 views

STM32CubeIDE v1.12.0

This type question has been asked different ways but never specifically for a procedure. In the past we have used Eclipse Workspaces with a single project and we were able to copy, paste and rename the Workspace and then open it as a different Worspace without issues. Attempting to do this in STM32CubeIDE results in a identical Workspace(except for the directory name) but with the Workspace location that can not be modified.

If you open the Project properties==>Resource, the Path of the project is relative to the Location(which is the Workspace location), but the Location(Workspace) is not. We have not found a way to modify this Location so the Workspace/Project now has a fixed Location in the original users path.

  • Is there a way other than exporting the entire Project to change this?
  • Why is this Location locked? This breaks our code control methods.

Thanks

This topic has been closed for replies.

4 replies

CharlieMangold
Senior
May 31, 2023

After digging in the Properties=>Resource=>Linked Resources=>Path Variables, the "PROJECT_LOC" appears to be the original directory that had been copied. The PARENT_LOC, and WORKSPACE_LOC are the new directory. If you search through all the files in the new Workspace, there is only one that contains the text "PROJECT_LOC":

C:\Temp\Workspace\.metadata\.plugins\org.eclipse.core.runtime\.settings\org.eclipse.core.resources.prefs

Modifying the PROJECT_LOC path in this file does not make a difference after reopening the Workspace. 

CharlieMangold
Senior
May 31, 2023

Properties=>C/C++ General, click on Configure Workspace Settings, new window.

Preferences=>General=>Workspace=>Linked Resources.

This page shows a PROJECT_LOC. Modifying the org.eclipse.core.resources.prefs file causes changes here. Not sure why the PROJECT_LOC variable listed in the Project properties==>Resource=>Linked Resources=>Path Variables does not match.

CharlieMangold
Senior
June 1, 2023

We just check a different company project the uses STM32CubeIDE v1.9.0 and the Workspace copy/paste method works correctly. PARENT_LOC, PROJECT_LOC and WORKSPACE_LOC all use the same Workspace directory(the PROJECT_LOC also tags on the Project directory.) Is this a STM32CubeIDE version issue or is it something about the way the original project was created? Can someone from ST tell us why the PROJECT_LOC is locked or maybe why that would happen?

Thanks.


_legacyfs_online_stmicro_images_0693W00000dJpi3QAC.png 

CharlieMangold
Senior
June 30, 2023

Just to close this out we ended up taking this project and re-importing it into a new one. After the import was done, PARENT_LOC, PROJECT_LOC and WORKSPACE_LOC all use the new Workspace directory.