Skip to main content
Jack3
Senior
May 1, 2026 1:42 PM UTC
Question

STM32CubeIDE keeps collapsing the Project Explorer

In STM32CubeIDE 2.1.1, Project Explorer keeps collapsing constantly.

This has been a persistent bug for a very long time and is very annoying.

Can't ST just fix this since it is based on Eclipse?

3 replies

Ghofrane GSOURI
ST Technical Moderator
May 4, 2026 9:56 AM UTC

Hello @Jack3 

The recommended solution is to create a new STM32CubeIDE workspace, because this is the safest and most effective way to remove corrupted UI or metadata state without touching the actual project files.

Go to  File → Switch Workspace  ,select a new empty workspace from this menu, restart STM32CubeIDE in that fresh workspace, and then re-import the existing project.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Jack3
Jack3Author
Senior
Jul 3, 2026 9:08 AM UTC

That doesn't work, because the problem always pops up again shortly afterwards.

It is better to fix that bug anyway.

Ghofrane GSOURI
ST Technical Moderator
Jul 3, 2026 9:13 AM UTC

Hello ​@Jack3 

The STM32CubeIDE 2.2.0 is now available.

Could you please try it and confirm whether the issue still occurs?

Download STM32CubeIDE from here 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.