Skip to main content
RMack.1
Associate
March 10, 2023
Question

STM32CubeIDE issue initializing Debugging

I have been having this issue reoccuring and has only started in the past month. I have upgrade and downgraded versions (currently back at 1.12.0) with hopes to fix it and while it goes away for a bit and I am able to work with the live debugging for a bit it always returns.

The two behaviours are giving me an error with the register 0 or the following:

"Board    : STLINK-V3SET

Voltage   : 3.28V

SWD freq  : 8000 KHz

Connect mode: Under Reset

Reset mode : Hardware reset

Device ID  : 0x450

Revision ID : Rev V

Device name : STM32H7xx

Flash size : 2 MBytes

Device type : MCU

Device CPU : Cortex-M7

BL Version : 0x90

Memory Programming ...

Opening and parsing file: ST-LINK_GDB_server_a07300.srec

 File     : ST-LINK_GDB_server_a07300.srec

 Size     : 110.96 KB 

 Address    : 0x08020000 

Erasing memory corresponding to segment 0:

Erasing internal memory sector 1

Download in Progress:

File download complete

Time elapsed during download operation: 00:00:01.236

Verifying ...

Download verified successfully 

Shutting down...

Exit."

I usually can get this issue to go away after playing around with the Debug Configurations, but so far nothing reproducible.

This topic has been closed for replies.

3 replies

Rim LANDOLSI
ST Employee
March 13, 2023

Hello @RMack.1​ ,

At first, let me thank you for reporting this issue.

Are you using the right debug buttom and not the run buttom. Because, everything is downloaded successfully.

0693W00000aInnlQAC.png 

Thanks,

Rim

RMack.1
RMack.1Author
Associate
March 15, 2023

Yes I am sure I am selecting the "Debug"

So far I am able to resolve this issue by comparing the ".launch" files for a previously working file but I am still not sure why it would be changing this file's settings. The alternative error it has been getting is:

"Failed to assign value 80224ed, to register 0

Failed to assign value 240375f8, to register 0

Failed to assign value 2407fff8, to register 0

Failed to assign value 803f332, to register 0"

It seems to happen after a crash of the IDE but still seems to be altering the launch settings for the debugging.

Rim LANDOLSI
ST Employee
March 16, 2023

Hello @RMack.1​ ,

Could you, please, provide :

  • CubeIDE version that you have upgraded from
  • Microcontroller
  • Debug configuration
  • Live debugging window used for this example

It would be, also, helpful to provide the whole projects you are working on .