Skip to main content
ADaxa.1
Associate II
Jan 2, 2021 2:25 PM UTC
Question

STM32CubeIDE is not connecting to the internet.

I had several versions of the IDE installed on my machine but none of them could connect to the internet to update or load code. I keep getting the error message "In order to benefit from best experience a network connection is required. Do you want to set connection parameter now?". At first I thought it was because Norton was blocking the the applications through the firewall but I uninstalled Norton and installed the IDE again but that didn't fix the problem. I installed the IDE on my brothers machine which doesn't have Norton and it worked fine on there. I also have used different networks in the past 2 months so that cant be it. Can anyone please help?

16 replies

Peter BENSCH
ST Technical Moderator
Jan 4, 2021 10:26 AM UTC

What are your settings in

  • Window > Preferences > Network Connections
  • Window > Preferences > STM32Cube > Firmware Updater?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ADaxa.1
ADaxa.1Author
Associate II
Jan 4, 2021 1:06 PM UTC

0693W000006HPleQAG.jpg

Peter BENSCH
ST Technical Moderator
Jan 4, 2021 3:57 PM UTC

What about the settings from the first point (Network Connections)?

You can also reach them by clicking Network Connections in the screen above.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ADaxa.1
ADaxa.1Author
Associate II
Jan 4, 2021 6:06 PM UTC

0693W000006HTJZQA4.jpg

Peter BENSCH
ST Technical Moderator
Jan 5, 2021 1:57 PM UTC

Setting the Active Provider to Native is usually fine.

If you are connected to the Internet without a proxy, you can test whether setting to Direct is working for you. Please Apply after setting and test the connection using Check Connection in Firmware Updater.

Instead set Active Provider to Manual and set the required parameters (host, port, user, pwd) if you are behind a proxy. It might also be a good idea to set these parameters and test Active Provider with Native again.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ADaxa.1
ADaxa.1Author
Associate II
Jan 5, 2021 4:19 PM UTC

I tried your suggestions and nothing seems to have changed. Ill try to contact Microsoft to try to resolve the problem. Thanks for your help anyways.

KHe.1
Associate
Aug 18, 2023 8:43 PM UTC

Hi ADaxa.1, 

Did you resolve it? How did you make it to work? I have the same issue. Thank you!

Associate III
Jan 11, 2024 10:32 PM UTC

I had the same problem and solved it by changing Active Provider to Direct.

 

Clyde_S_0-1705012346706.png

 

Visitor II
Sep 20, 2024 4:23 PM UTC

I am having a connection issue from my new company laptop, and no settings seem to work for me (same problem in both CubeMx and CubeIde). I should also note that I have NO problems working off the same (home) network from my personal PC.

I looked in the CubeIde .log file and found the following java exception, but not sure if it means that I have an issue or ST has a certificate issue.  The log contained this:

ENTRY org.eclipse.equinox.p2.transport.ecf 4 1002 2024-09-20 10:35:42.036
!MESSAGE Unable to read repository at https://sw-center.st.com/stm32cubeide/updatesite1/content.xml.
!STACK 0
javax.net.ssl.SSLHandshakeException: PKIX path building failed: sun.security.provider.certpath.SunCertPathBuilderException: unable to find valid certification path to requested target
at java.base/sun.security.ssl.Alert.createSSLException(Alert.java:131)
at java.base/sun.security.ssl.TransportContext.fatal(TransportContext.java:378)
at java.base/sun.security.ssl.TransportContext.fatal(TransportContext.java:321)
at java.base/sun.security.ssl.TransportContext.fatal(TransportContext.java:316)
at java.base/sun.security.ssl.CertificateMessage$T13CertificateConsumer.checkServerCerts(CertificateMessage.java:1351)
at java.base/sun.security.ssl.CertificateMessage$T13CertificateConsumer.onConsumeCertificate(CertificateMessage.java:1226)
at java.base/sun.security.ssl.CertificateMessage$T13CertificateConsumer.consume(CertificateMessage.java:1169)
at java.base/sun.security.ssl.SSLHandshake.consume(SSLHandshake.java:396)
at java.base/sun.security.ssl.HandshakeContext.dispatch(HandshakeContext.java:480)
at java.base/sun.security.ssl.SSLEngineImpl$DelegatedTask$DelegatedAction.run(SSLEngineImpl.java:1277)
at java.base/sun.security.ssl.SSLEngineImpl$DelegatedTask$DelegatedAction.run(SSLEngineImpl.java:1264)
at java.base/java.security.AccessController.doPrivileged(AccessController.java:712)
at java.base/sun.security.ssl.SSLEngineImpl$DelegatedTask.run(SSLEngineImpl.java:1209)
at java.base/java.util.ArrayList.forEach(ArrayList.java:1511)
at java.net.http/jdk.internal.net.http.common.SSLFlowDelegate.lambda$executeTasks$3(SSLFlowDelegate.java:1118)
at java.net.http/jdk.internal.net.http.HttpClientImpl$DelegatingExecutor.execute(HttpClientImpl.java:157)
at java.net.http/jdk.internal.net.http.common.SSLFlowDelegate.executeTasks(SSLFlowDelegate.java:1113)
at java.net.http/jdk.internal.net.http.common.SSLFlowDelegate.doHandshake(SSLFlowDelegate.java:1079)
at java.net.http/jdk.internal.net.http.common.SSLFlowDelegate$Reader.processData(SSLFlowDelegate.java:484)
at java.net.http/jdk.internal.net.http.common.SSLFlowDelegate$Reader$ReaderDownstreamPusher.run(SSLFlowDelegate.java:268)
at java.net.http/jdk.internal.net.http.common.SequentialScheduler$LockingRestartableTask.run(SequentialScheduler.java:205)
at java.net.http/jdk.internal.net.http.common.SequentialScheduler$CompleteRestartableTask.run(SequentialScheduler.java:149)
at java.net.http/jdk.internal.net.http.common.SequentialScheduler$SchedulableTask.run(SequentialScheduler.java:230)
at java.base/java.util.concurrent.ThreadPoolExecutor.runWorker(ThreadPoolExecutor.java:1136)
at java.base/java.util.concurrent.ThreadPoolExecutor$Worker.run(ThreadPoolExecutor.java:635)
at java.base/java.lang.Thread.run(Thread.java:840)
Caused by: sun.security.validator.ValidatorException: PKIX path building failed: sun.security.provider.certpath.SunCertPathBuilderException: unable to find valid certification path to requested target
at java.base/sun.security.validator.PKIXValidator.doBuild(PKIXValidator.java:439)
at java.base/sun.security.validator.PKIXValidator.engineValidate(PKIXValidator.java:306)
at java.base/sun.security.validator.Validator.validate(Validator.java:264)
at java.base/sun.security.ssl.X509TrustManagerImpl.checkTrusted(X509TrustManagerImpl.java:285)
at java.base/sun.security.ssl.X509TrustManagerImpl.checkServerTrusted(X509TrustManagerImpl.java:144)
at java.base/sun.security.ssl.CertificateMessage$T13CertificateConsumer.checkServerCerts(CertificateMessage.java:1329)
... 21 more
Caused by: sun.security.provider.certpath.SunCertPathBuilderException: unable to find valid certification path to requested target
at java.base/sun.security.provider.certpath.SunCertPathBuilder.build(SunCertPathBuilder.java:148)
at java.base/sun.security.provider.certpath.SunCertPathBuilder.engineBuild(SunCertPathBuilder.java:129)
at java.base/java.security.cert.CertPathBuilder.build(CertPathBuilder.java:297)
at java.base/sun.security.validator.PKIXValidator.doBuild(PKIXValidator.java:434)
... 26 more

mattias norlander
ST Technical Moderator
Aug 24, 2023 7:48 AM UTC

Would be interesting to see if you have any log messages that we can associate with these problems.

Please have a look your workspace\.metadata\

You should find two files:

  • One called .log, produced by CubeIDE/Eclipse/...
  • Another called ide.log, produced by CubeMX

Can you have a look at these logs? When doing that try again to perform the log-in and notice exactly at what time you did the log-in attempt in order to be able to map the time with the time stamps in the log-files. Then we should know exactly which log-messages (if any) was produced by the log-in feature...

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Explorer
Nov 5, 2024 8:48 AM UTC

Hello, I am also experiencing issue trying to connect to the Internet(version 1.16 of the CubeIDE on Windows11). I tried all suggested actions but without success. I also tried using an Internet cable which allows connection to Internet from the IDE on other PC - which should eliminate the possibility to have incorrect internet/proxy settings on mine. From the ide.log , when trying to login I get: UserAuth:417 - Internet connection configuration mode: 2