Skip to main content
Associate II
Aug 29, 2025 7:39 AM UTC
Question

STM32CubeIDE: HSI → PLL /2 not honored (Nucleo-F303RE, expected 36 MHz but runs at 72 MHz)

Hi Team,

I’m prototyping on a Nucleo-F303RE using STM32CubeIDE. In the clock configuration, I set the system clock to 36 MHz from HSI (HSI → PLL with the /2 divider), as shown in the clock tree screenshot.

 

Bhavil_0-1756452511992.png

However, my firmware misbehaved. After debugging, I found that SystemClock_Config() function isn’t applying the HSI/2 divider when feeding the PLL. Instead of:

 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;

CubeIDE generates:

 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI_DIV2;

 

This effectively makes the system clock 72 MHz instead of the configured 36 MHz.

Did I misconfigure something in the clock setup, or is this a CubeIDE code-generation bug when using HSI with the PLL /2 divider?

5 replies

ST Technical Moderator
Aug 29, 2025 8:57 AM UTC

Hello @Bhavil 

What is the version of the firmware and STM32CubeIDE used? 

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
BhavilAuthor
Associate II
Aug 29, 2025 9:19 AM UTC

Hi @Souhaib MAZHOUD 

I am currently on Version 1.19.0. 

Bhavil_0-1756459088328.png

I am a little unsure, regarding the firmware version. Can you help me where I can find that?

BhavilAuthor
Associate II
Sep 1, 2025 5:44 AM UTC

Hi @Souhaib MAZHOUD ,

Do you have any updates?

Also a little but vital edit in the question

The CubeIDE generates 

RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;

instead of 

RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI_DIV2;


I jumbled it up while posting the question

ST Technical Moderator
Sep 5, 2025 2:07 PM UTC

Hello @Bhavil 

Actually RCC_PLLSOURCE_HSI_DIV2 is not defined in stm32f303xe.h, Therefore, I suggest that you use HSI as input for PLL Source and Prediv /2 to address your clock configuration.
Meanwhile, this issue has been raised to the development team for analysis and revision of upcoming releases (Ticket 216974 This is an internal tracking number and is not accessible or usable by customers).)

KR,

Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.