Skip to main content
stanley.setiawan
Associate II
January 3, 2024
Solved

STM32CubeIDE Headless build in CI/CD

I'm trying to perform a headless build for our gitlab's pipeline. However, I encountered some problems with it.

Firstly, I want to mention that the build process went smoothly before, but then as I need to change the name of the project, problem arises with the pipeline.

 

So far, I have managed to change all the required changed in the .cproject, .project and other references to the old project name. Hence, when I tried to perform a build and even a debug session from my PC, it went perfectly fine, without any problems. 

The same goes with building the project via a headless build process manually from a linux machine (the docker image of my pipeline). However, when I tried to run it automatically from Gitlab's runner, it failed saying:

 

 

URI: file:/builds/6tyu7Drk/0/path/projName is not valid in the workspace!

 

 

 

The steps for my successful manual headless build:

 

 

git clone http://address_of_repo/projName.git /builds/6tyu7Drk/0/path/projName
cd /builds/6tyu7Drk/0/path/projName
git checkout BRANCH_NAME
/opt/st/stm32cubeide_1.10.1/headless-build.sh -import .
/opt/st/stm32cubeide_1.10.1/headless-build.sh -cleanBuild ProjName

 

 

 

The YAML file for my unsuccessful build:

 

 

/opt/st/stm32cubeide_1.10.1/headless-build.sh -import . #creates a workspace

 

 

the response from the build server is:

 

 

Running with gitlab-runner 16.7.0 (xxxxxx)
 on build server 6tyu7Drk, system ID: s_dddddddddddd
Preparing the "shell" executor
Using Shell (bash) executor...
Preparing environment
Running on ddddddddd...
Getting source from Git repository
Fetching changes...
Initialized empty Git repository in /builds/6tyu7Drk/0/path/projName/.git/
Created fresh repository.
Checking out af7ab01a as detached HEAD (ref is refs/merge-requests/131/head)...
$ cd $CI_PROJECT_DIR
$ /opt/st/stm32cubeide_1.10.1/headless-build.sh -import .
URI: file:/builds/6tyu7Drk/0/path/projName is not valid in the workspace!
Stm32cubeide:
JVM terminated. Exit code=1
/opt/st/stm32cubeide_1.10.1//plugins/com.st.stm32cube.ide.jre.linux64_2.2.0.202203101208/jre/bin/java
-Dosgi.requiredJavaVersion=1.8
-Dosgi.instance.area.default=@user.home/STM32CubeIDE/workspace_1.10.1
-Declipse.buildId=Version 1.10.1
-DproductMaturityGrade=mm
-XX:+UseG1GC
-XX:+UseStringDeduplication
-Xms256m
-Xmx1024m
-jar /opt/st/stm32cubeide_1.10.1//plugins/org.eclipse.equinox.launcher_1.6.400.v20210924-0641.jar
-os linux
-ws gtk
-arch x86_64
-launcher /opt/st/stm32cubeide_1.10.1/stm32cubeide
-name Stm32cubeide
--launcher.library /opt/st/stm32cubeide_1.10.1//plugins/org.eclipse.equinox.launcher.gtk.linux.x86_64_1.2.400.v20211117-0650/eclipse_11600.so
-startup /opt/st/stm32cubeide_1.10.1//plugins/org.eclipse.equinox.launcher_1.6.400.v20210924-0641.jar
--launcher.overrideVmargs
-exitdata 23
-application org.eclipse.cdt.managedbuilder.core.headlessbuild
-import .
-vm /opt/st/stm32cubeide_1.10.1//plugins/com.st.stm32cube.ide.jre.linux64_2.2.0.202203101208/jre/bin/java
-vmargs
-Dosgi.requiredJavaVersion=1.8
-Dosgi.instance.area.default=@user.home/STM32CubeIDE/workspace_1.10.1
-Declipse.buildId=Version 1.10.1
-DproductMaturityGrade=mm
-XX:+UseG1GC
-XX:+UseStringDeduplication
-Xms256m
-Xmx1024m
-jar /opt/st/stm32cubeide_1.10.1//plugins/org.eclipse.equinox.launcher_1.6.400.v20210924-0641.jar 
ERROR: Job failed: exit status 1

 

 

 

Can anyone help me with this issue? Thanks!

 

BR,

S

This topic has been closed for replies.
stanley.setiawan
stanley.setiawanBest answer
Associate II
January 4, 2024

Solved by reinstalling the docker image. For some reason, the old built data is somehow still stored there, hence there is a conflict that I couldn't understand. Hence, by reinstalling the docker image, the build was ok.

1 reply

stanley.setiawan
stanley.setiawanAuthorBest answer
Associate II
January 4, 2024

Solved by reinstalling the docker image. For some reason, the old built data is somehow still stored there, hence there is a conflict that I couldn't understand. Hence, by reinstalling the docker image, the build was ok.