Skip to main content
Adrian Adamson
Senior
May 23, 2022 5:51 PM UTC
Question

STM32CubeIDE Failed to execute MI command: load

I have been developing successfully with STM32CubeIDE for several years. My current project has been going ok, with lots of in-application debugging, until my latest revision. The debugger quits with the following error message:

----------------------------------

Error in final launch sequence:

Failed to execute MI command:

load C:\\Users\\feath\\OneDrive\\Documents\\Featherweight\\BlueRaven\\IDE_Workspace\\BlueRaven\\Debug\\BlueRaven.elf 

Error message from debugger back end:

You can't do that when your target is `exec'

Failed to execute MI command:

load C:\\Users\\feath\\OneDrive\\Documents\\Featherweight\\BlueRaven\\IDE_Workspace\\BlueRaven\\Debug\\BlueRaven.elf 

Error message from debugger back end:

You can't do that when your target is `exec'

Failed to execute MI command:

load C:\\Users\\feath\\OneDrive\\Documents\\Featherweight\\BlueRaven\\IDE_Workspace\\BlueRaven\\Debug\\BlueRaven.elf 

Error message from debugger back end:

You can't do that when your target is `exec'

You can't do that when your target is `exec'

--------------------------------------

I can revert to a previous revision of code, which is identical except for an unused index variable, and it debugs fine.

I have tried all combinations of unplugging/re-plugging, quits and computer restarts, and I consistently get the problem with my latest revision but not the previous rev.

I saved off the debugger log for the working case and the non-working case, and when I review them, there's nothing that jumps out at me as the problem for why the debugger gives up, but I don't know what most of the log entries mean.

Anyone have any insight?

For the moment I'm making a new branch from my previous revision and trying to work from there, but I'm afraid the same thing will pop up again.

7 replies

Adrian Adamson
Senior
May 23, 2022 6:40 PM UTC

Update: The second-most-recent code version has the same problem, and also going back a few versions. I basically can't use the IDE for any in-circuit debugging right now.

Adrian Adamson
Senior
May 23, 2022 9:40 PM UTC

As another datapoint, when I run the same project from a different computer (the project is located in OneDrive), it debugs fine. Maybe I need to re-install STM32Cube_IDE?

Adrian Adamson
Senior
May 23, 2022 10:33 PM UTC

Update: I re-installed STM32Cube_IDE, and voila, I can debug my project now. Then I had to go back and re-fix the icon size, and re-install EGIT. Unfortunately, the egit installation has not been successful. I tried uninstalling and re-installing, and I just have red x's where I should have the staging view, etc.

Adrian Adamson
Senior
Jun 16, 2022 4:29 PM UTC

The problem is back again. I think I will write a support ticket.

Adrian Adamson
Senior
Oct 29, 2024 4:23 PM UTC

The problem popped up again. I should have written down how I got past this in 2022.

Adrian Adamson
Senior
Oct 29, 2024 10:28 PM UTC

I got past it today after numerous restarts, reboots, power cycling the STlink, changing USB ports, etc.  Several hours worth where it would work maybe 1 out of 5 tries.   Eventually it started working all the time again.    I think a common thread when this happens over the years is that I accidentally set too many breakpoints shortly before the failure starts happening.   Today a contributing factor may have been having too many USB ports open due to running a bunch of parallel STLinks on my production programming and test fixture.

Explorer
Jan 20, 2026 1:43 AM UTC

Hi Adrian

I encountered maybe the same problem with you.  

My setup is
IDE: S32DS
Development board: S32K324
And i tried several methods as below
1.  check the  power
2. check the wheather the interface is plugged
3. restart my PC

4. close all breakpoints

And it still didn't work. It will be appreciated if you can help me analysize the log 

Valent_0-1768873120720.jpg