Skip to main content
Jwu.6
Associate
Mar 24, 2021 2:00 AM UTC
Solved

STM32CubeIDE example GPIO_IOToggle_TrustZone ,Error: Data mismatch found at address 0x0C000000 (byte = 0xFF instead of 0x00)

Hi,

I try to run GPIO\GPIO_IOToggle_TrustZone in the STM32CubeIDE, but fail.

​

code:

STM32Nucleo\STM32Cube_FW_L5_V1.4.0\Projects\NUCLEO-L552ZE-Q\Examples\GPIO\GPIO_IOToggle_TrustZone

​

Follow the readme steps without modifying any code or configuration。

After build, Select the xxxxx_S project and select "Debug ,select startup , add NS project

Fail at download:

Error: Data mismatch found at address 0x0C000000 (byte = 0xFF instead of 0x00)

​

The others example without TZ run OK.

This is my first time to use this platform. Is there anything else that needs to be configured, or something wrong with the operation,

​

Console output:

Erasing memory corresponding to segment 0:

Erasing internal memory sectors [0 4]

Erasing memory corresponding to segment 1:

Erasing internal memory sector 124

Download in Progress:

​

​

File download complete

Time elapsed during download operation: 00:00:00.328

​

​

​

Verifying ...

​

​

​

​

Error: Data mismatch found at address 0x0C000000 (byte = 0xFF instead of 0x00)

​

​

Error: Download verification failed

​

​

Encountered Error when opening D:\software\ST\STM32CubeIDE_1.6.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_1.6.0.202101291314\tools\bin\STM32_Programmer_CLI.exe

Error in STM32CubeProgrammer

Debugger connection lost.

Shutting down...

This topic has been closed for replies.
Jwu.6
Jwu.6Best answer
Associate
Mar 24, 2021 2:59 AM UTC

Find the cause of the problem, need to do some basic configuration, after config, it works ok

​

To match the default partitioning, the STM32L5xx Series devices must have the following user option bytes set:

TZEN=1 (TrustZone-enabled device)

DBANK=1 (Dual bank Flash configuration)

SECWM1_PSTRT=0x0 SECWM1_PEND=0x7F (all 128 pages of Flash Bank1 set as secure)

SECWM2_PSTRT=0x1 SECWM2_PEND=0x0 (no page of Flash Bank2 set as secure, hence Bank2 is non-secure)

1 reply

Jwu.6
Jwu.6AuthorBest answer
Associate
Mar 24, 2021 2:59 AM UTC

Find the cause of the problem, need to do some basic configuration, after config, it works ok

​

To match the default partitioning, the STM32L5xx Series devices must have the following user option bytes set:

TZEN=1 (TrustZone-enabled device)

DBANK=1 (Dual bank Flash configuration)

SECWM1_PSTRT=0x0 SECWM1_PEND=0x7F (all 128 pages of Flash Bank1 set as secure)

SECWM2_PSTRT=0x1 SECWM2_PEND=0x0 (no page of Flash Bank2 set as secure, hence Bank2 is non-secure)