Hello @eduardo_reis
The error "Error downloading the following files: mcusAds.json.tmp (Not available)" in STM32CubeIDE 1.19.0 usually occurs due to network connectivity issues, firewall or proxy restrictions, or temporary server unavailability when the IDE tries to download necessary package files. To resolve this, make sure your internet connection is stable, configure any proxy settings within the IDE if needed, and check that no firewall or antivirus is blocking the download. Clearing the IDE’s cache (.stm32cubeide) can also help. Running the IDE with administrator privileges may resolve permission-related problems.
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.