Skip to main content
MRahi.3
Associate II
June 8, 2021
Question

STM32CubeIDE debugging problem : Error in final launch sequence

Hello, I am currently trying to program an STEVAL-ESC001v1 board with an STLINK V2 ISOL probe. The IDE I use is the STM32CubeIDE. Before that, I used a regular STLINK V2 probe and the debugging of my program worked perfectly. Ever since I switched to the STLINK V2 ISOL (for isolation from power), I have been getting these errors on the console :

STMicroelectronics ST-LINK GDB server. Version 5.8.0

Copyright (c) 2020, STMicroelectronics. All rights reserved.

Starting server with the following options:

    Persistent Mode      : Disabled

    Logging Level       : 1

    Listen Port Number     : 61234

    Status Refresh Delay    : 15s

    Verbose Mode        : Disabled

    SWD Debug         : Enabled

    InitWhile         : Enabled

Waiting for debugger connection...

Debugger connected

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Debugger connection lost.

Shutting down...

0693W00000BaQ4tQAF.png 

I tried using the STM32CubeProgrammer software, but It seems like the ISOL probe doesn't recognize the target :

0693W00000BaQCJQA3.png0693W00000BaQCTQA3.png 

Can anyone help me out with this issue ? Thank you very much

This topic has been closed for replies.