Skip to main content
Associate II
Jul 23, 2025 2:44 PM UTC
Question

STM32CubeIDE debugging not starting

Hello,

I recently run into problem with not being able to debug my applications any more.

I use STM32CubeIDE (and Atollic) without major problems for years now, but suddenly debugging does not start.

I can flash the the device through the Run button. When I click debug it is also flashed but than progress stops at around 95% percent and stays there forever. Logs do not look the same every time so just some examples here.

JeronymJ_1-1753281198591.png

JeronymJ_3-1753281431206.png

 

 

I tested multiple applications with 3 programmers  (ST link V2, ST-link V2 from 3rd party, ST-link on Nucleo Board) connected to multiple custom devices that previously worked. I use 4-wire programming (V, SWDIO,SWCLC,GND)

However when using Nucleo board directly it starts normally.

I experimented with dubug configurations, reinstalled the IDE, drivers, tried older versions, nothing seems to make a difference.

Thank you for the support.

regards Jeronym

 

 

This topic has been closed for replies.

1 reply

JeronymJAuthor
Associate II
Jul 23, 2025 3:07 PM UTC

Some new information. After i run my test program on Nucleo Board (and it worked as mentioned before), iI than could also debug with the same programmer using other custom HW, than I tested the other ST-link V2 and it works as well.
So it seems running debugging on Nucleo board once fixed the problem for other boards and programmers.

However I do not consider the issue solved, because I am almost sure it will come back again. I think this already happened once before and stopped working the day after...