Skip to main content
Proteus
Associate II
April 15, 2021
Question

STM32CUBEIDE DEBUG PROBLEM

Hello

My debugger is shutting down after downloading code into chip 

I can connect STLINK UTILITY and uploading code hex files properly

STMicroelectronics ST-LINK GDB server. Version 5.8.0
Copyright (c) 2020, STMicroelectronics. All rights reserved.
 
Starting server with the following options:
 Persistent Mode : Disabled
 Logging Level : 1
 Listen Port Number : 61234
 Status Refresh Delay : 15s
 Verbose Mode : Disabled
 SWD Debug : Enabled
 
Waiting for debugger connection...
Debugger connected
 -------------------------------------------------------------------
 STM32CubeProgrammer v2.7.0-RC1 
 -------------------------------------------------------------------
 
ST-LINK SN : 50FF6D064965575354401887
ST-LINK FW : V2J37S0
Board : --
Voltage : 2.89V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x445
Revision ID : Rev 1.0
Device name : STM32F04x/F070x6
Flash size : 32 KBytes
Device type : MCU
Device CPU : Cortex-M0
 
 
 
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a14724.srec
 File : ST-LINK_GDB_server_a14724.srec
 Size : 27540 Bytes
 Address : 0x08000000 
 
 
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 26]
Download in Progress:
 
 
File download complete
Time elapsed during download operation: 00:00:01.764
 
 
 
Verifying ...
 
 
 
 
Download verified successfully 
 
 
Debugger connection lost.
Shutting down...

This topic has been closed for replies.

1 reply

Proteus
ProteusAuthor
Associate II
April 16, 2021

Is there any recommendation ?