Skip to main content
BRobe.1641
Associate II
Jan 28, 2023 4:34 PM UTC
Question

Stm32CubeIDE crashes on startup: "Java" is not responding

My linux laptop (Ubuntu 22.04) failed to properly 'sleep' overnight - there is something wrong with the install of Ubuntu on my laptop. At the time, CubeIDE 1.11.2 was running, with Devstyle plugin (which has itself caused problems for me in the past). I have tried removing the 'st' folder in /opt, and reinstalling, and that had no impact. While this may just be a problem with my system76 linux laptop, other applications appear to be functioning normally.

To clarify, when I load STM32CubeIDE, the devstyle splash screen came up, and then after I proceed into the IDE, it freezes, with a message that says "Java" is not responding. On starting up since, I have skipped the devstyle splash screen, and instead get the blue-colored splash of CubeIDE - but it just freezes, saying the same thing, and suggesting I force quit.

Is there a way to diagnose this problem?

This topic has been closed for replies.

15 replies

Maposaagsky
Associate II
Mar 19, 2025 4:58 PM UTC

 

Eliminar toda la carpeta workbench (si sigue fallando)
Si el IDE sigue sin funcionar, prueba eliminando toda la carpeta: