Here on my (new) MxLinux and IDE 1.17.0 :
arm-none-eabi-size mini-DSO-F303-ili9341.elf
arm-none-eabi-objcopy -O binary mini-DSO-F303-ili9341.elf "mini-DSO-F303-ili9341.bin"
text data bss dec hex filename
42604 480 19860 62944 f5e0 mini-DSO-F303-ili9341.elf
Finished building: default.size.stdout
Finished building: mini-DSO-F303-ili9341.bin
12:28:53 Build Finished. 0 errors, 1 warnings. (took 677ms)
So this is what you can expect - if everything working fine (AMD Ryzen and with SSD/M2 disc). :D
At first i had installed EndeavourOS - but got about 1...3 minutes to compile !
So i tried to find the reason - and its not the IDE itself, its a call to something like "check all open files in system".
Problem is: on many systems this defaults to max.open files, big number. To limit it, call:
ulimit -n -H 4096
(https://www.reddit.com/r/debian/comments/1einvq3/solved_problems_with_the_newest_stm32cubeide_on/ )
Please remember that this command modifies the settings only for that particular console session. So you need to run CubeIDE from the command line, in the same console session.
I usually use the following script for that (the /home/emb/st/bin is the directory where I have put the stlink-server binary).
#!/bin/bash
(
export PATH=/home/emb/st/bin:$PATH
ulimit -n -H 4096
/home/emb/st/stm32cubeide_1.17.0/stm32cubeide
)
So with limit to open files its running ok then.
Just on MxLinux they have set a useful limit and so IDE just running without extra delay.
Try.
(Next problem you might see, when start debug...but thats another story.
see:
https://community.st.com/t5/stm32cubeide-mcus/on-ubuntu-debug-says-quot-could-not-determine-gdb-version-quot/m-p/761775#M33561
)
If you feel a post has answered your question, please click on " Best Answer ".