STM32CubeIDE build (Make) incredibly slow
Hello,
I created a project with many C files (around 50 or 60) and the build is incredibly slow. I'm just doing "build project", and even when nothing changed in the project, it takes several MINUTES just to start compiling the few modified C files.
The build command line is supposed to be "make -j2 all" but it apparently takes forever before it is actually executed.
Any hint ?
EDIT: I tried to execute the make command outside the IDE but I get an error "multiple target patterns". I have to mention that the source file are on a linux server whose disk is mounted on my windows PC. I tried the make directly on the linux server which may explain the issue.