Skip to main content
F F
Associate III
Dec 8, 2022 1:11 PM UTC
Solved

STM32CubeIDE broke after update v1.11.0!

I just migrated to the latest v1.11 of STM32CubeIDE.

I was able to update successfully to the latest version, but now my environment is broken!

Issues I see now:

  • Build an stack analyzer gives the following output:

Could not create the view: com.st.stm32cube.ide.mcu.stackanalyzer.stackanalyzer.view

  • Unable to open the dedicated .ioc file:

Gives an NullPointerException

Also I'm unable to restore my environment downloading the latest installer file. The website is having issues and I'm unable to login / download content disappears after login.

Please ST help me with an urgent workaround!

EDIT: Website back online, "solved" by using the installer of v1.11. Please fix this ST!

Regards,

This topic has been closed for replies.
Markus GIRDLAND
Markus GIRDLANDBest answer
ST Employee
Dec 13, 2022 9:25 AM UTC

Copy-pasted from another thread:

Hello there!

I'm fairly certain that you are facing the new issue that my colleague Mattias is mentioning in this thread:

https://community.st.com/s/question/0D53W00001zeSZcSAM/stm32cubeide-intool-update-issue

It might work if you remove CDT from the available software sites:

0693W00000WKsYFQA1.png 

We are currently investigating this issue further!

21 replies

raimund.532595229839029E12
Visitor II
Dec 13, 2022 5:04 PM UTC

Hello users,

i can confirm this behavior.

Some days ago, maybe a week, on my desktop, i did a "parallel" fresh install of 1.11.0, to an existing 1.10.x. Then i added 2 older toolchains, and this worked.

Last Thursday, i tried to do the same on my Laptop. Fresh install of 1.11.0, this works. After adding older toolchains, errors like described. Removing 1.11.0, then upgrading the existing 1.10.x (already with the two older toolchains) on that Laptop to 1.11.0, IDE is broken. So no more working IDE on the Laptop.

Then removing all STM32CubeIDE´s and folders, and getting (just copying) the whole installation directory from my Desktop to the Laptop, same folders, same workspace directories, and that worked for me.

So my assumption is, that something is wrong with the installation sources in the web (now). Because before one week or so the process was working, at least for me..

DNiko.1
Associate
Dec 13, 2022 5:52 PM UTC

I've got same issue and I tried anything ... but it didn't help.

Then uninstalled it and did a fresh new install so all works again

Fendo59
Associate II
Dec 24, 2022 2:55 PM UTC

I tried to install STM32cubeide 1.11.0 on Ubuntu 22.04.1 LTS. When it proposes the license window, it is empty and I can't do anything anymore. I made various tests, following indications found on the web, without success.

I downloaded the installer again, nothing changed. Finally I installed STM32cubeide 1.10.1 and everything works fine on the first attempt.

I await the solution from ST.

Regards