Skip to main content
Jack3
Senior
April 26, 2019
Question

STM32CubeIDE - Auto-complete (Ctrl+Space) is not working

Hello, I installed STM32CubeIDE and imported (a copy) of a TS project.

Quickly, I hit an issue: auto-complete proposals (Ctrl+Space) gave no proposals in STM32CubeIDE. The pop-up window only shows 'No Default Proposals'

  

UPDATE: I fixed it, the preferences setting needed to be a little bit different than in TS.

In Preferences -> C/C++ -> Editor -> Content Assist -> Advanced

I checked the following boxes:

  • Parsing-based Proposals

Both in the upper and lower window.

Note, I imported my preferences settings from TS, as it is a huge task to manually get the IDE colors right, otherwise. I think this disabled the auto-complete feature (which worked in TS).

I hope this helps somebody, when hitting the same problem.

Some other remarks for who is interested.

I noticed it uses 'arm-none-eabi-gcc' instead of 'arm-atollic-eabi-gcc'.

The compilation time is about 30-50% longer (all threads enabled).

TS used to ignore changes in the header files, making a rebuild necessary in order to reflect any changes. This issue is solved in the new IDE!

  

This topic has been closed for replies.

14 replies

PWass
Associate
July 20, 2019

Thank you very much.:smiling_face_with_smiling_eyes: Had the same issue and it fixed it.

:grinning_face:

Greetings

zul-a
Visitor II
September 25, 2019

Thanks @Jack​ . Tonot have this checked by default is an offence..:grinning_face: ..

AlfaRomeo
Visitor II
April 8, 2020

Thank you Jack. It was very useful, I fix it finally. Kind regards :grinning_face_with_sweat:

haraldgraef
Associate
August 18, 2020

Thank you very much, @Jack​ ! Worked also for me. :grinning_face:

MrComrade
Visitor II
October 19, 2020

Thank You @Jack​ 

HSall.1
Visitor II
January 27, 2021

Thanks Jack

ad ho
Associate II
March 17, 2021

You saved my day and most of the following.

CLamb.1
Associate
March 22, 2021

Had the same problem with a fresh installation on a Mac... Your post saved my morning... Thank you!

Kepo
Visitor II
April 8, 2021

Thanks!