Skip to main content
Associate II
Dec 28, 2024 11:39 PM UTC
Question

STM32CubeIde and Error according extern"C"

I changed an example program for STM32F4 Discovery Board to C++ project.

When compiling the project, there are files included from BSP, which includes a definition:

extern "C".

When compiling the project, the first error is the following:

../../Drivers/BSP/STM32F4-Discovery/stm32f4_discovery.h:25:9: error: expected unqualified-id before string constant

25 | extern "C" {

| ^~~

what is the problem?

Thanks for responsing

This topic has been closed for replies.

5 replies

Tesla DeLorean
Guru
Dec 29, 2024 5:30 PM UTC

Any effort to prevent repeated inclusion of the same include file?

Closing brace matching?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
stefluikAuthor
Associate II
Dec 30, 2024 8:24 AM UTC

thanks for the reply.

I cannot see these issues as the problem.

There is only one include and the HAL files are from ST not manipulated.

Stefan

stefluikAuthor
Associate II
Dec 30, 2024 12:59 PM UTC

I think I found the more source of problem:

The code is a .c (C) file and it is compiled with gcc, not g++.

The project is set to C++.

All the HAL files are of course C-files.

But the code is compiled with the #define __cplusplus.

So of course the error pops up.

What is the correct solution?

I think one is to say, all .c files will be compiled with c++ compiler.

Is this correct direction?

Pavel A.
Dec 30, 2024 6:48 PM UTC

> Is this correct direction?

Short answer: no. 

Conversion of CubeIDE projects to C++ had been discussed here many times, please search. Rather won't start with that again.

stefluikAuthor
Associate II
Jan 12, 2025 10:13 PM UTC

Thanks for your reply.

Of course I tried searching. However, searching for C++ is not that easy.
I didn't find anything suitable.


I am very sad that you closed the post like this and no one replied to it or the solution is obviously in another post.


Apparently you are more intelligent than me and are hiding the solution to me and others by simply explaining it here.