Skip to main content
Ghofrane GSOURI
ST Technical Moderator
Jun 30, 2026 8:21 AM UTC
StickySolved

STM32CubeIDE 2.2.0 released

We are pleased to announce that STM32CubeIDE 2.2.0 release is now available. 

What is new in 2.2.0: 

  • Added support for: 

    •  STM32H5 microprocessors to the STM32H5 series   
    •  STM3U3 series microprocessors to the STM32U3 series  
    •  STM32V8 series 
  • Added support for new boards: 

    •  NUCLEO-H553ZG 
    •  NUCLEO-U345RC-Q, NUCLEO-U366RE-Q, STM32U366E-DK 
    •  NUCLEO-V873XJ, and STM32V873J-DK 
  • Updated the target Platform to Eclipse 2025-12 and CDT™ 12.3.0  
  • Added Multidrop support for debugging:  
    • STLINK-GDB server 
    • OpenOCD 
    • Segger J-Link 
  • Updated 

    • CMake to version 4.3.1  
    • STARM-CLANG to version 21.1.1+st.7  
    • Added support for 
    • OpenSTLinux 6.2.1  
    • CMake static library template  
    • Ubuntu 26.04 and Fedora 44  

Dependencies versions updates: 

  • Eclipse® 2025-12 and CDT™ version 12.3.0  

  •  Bundled JRE™: Adoptium® Temurin® 21.0.10+7 with JavaFX 21.0.10  

  • ST-LINK GDB Server 7.14.0 supporting ST-LINK/V2 and STLINK-V3  

  • SEGGER J-Link GDB Server V9.42 

  • STM32CubeProgrammer v2.23.0 

  • Open On-Chip Debugger 0.12.0+dev-00664-g72f14cee6 

  • RTOS Proxy 0.18.1 

  • Ninja 1.13.2  

  • make- 4.4.1_st_20260330-0700 

  • ST-LINK Server 2.1.2-2  

Main fixed issues in 2.2.0: 

Refer to the STM32 microcontroller wiki: here 

Known problems and limitations in 2.2.0: 

Refer to the STM32 microcontroller wiki: here 

How to get STM32CubeIDE 2.2.0: 

  • Download STM32CubeIDE from here 

  • Or update your current installation of STM32CubeIDE using: Help > Check for updates 

    • Note: 
      • The in-tool update does not update the drivers or the ST-LINK Server. A full installation is required to update all these components. 
This topic has been closed for replies.
Ghofrane GSOURI
Ghofrane GSOURIBest answer
ST Technical Moderator
Jul 6, 2026 9:38 AM UTC

This is an announcement post, if you have any issue or feedback to report please use the main page:

STM32CubeIDE (MCUs) | STM32 MCUs Software development tools | Community

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

Ghofrane GSOURI
Ghofrane GSOURIAuthorBest answer
ST Technical Moderator
Jul 6, 2026 9:38 AM UTC

This is an announcement post, if you have any issue or feedback to report please use the main page:

STM32CubeIDE (MCUs) | STM32 MCUs Software development tools | Community

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.