Skip to main content
EasyNet
Associate III
Dec 27, 2025 5:48 PM UTC
Question

STM32CubeIDE 2.0.0 Linux debugging issues and windows order breaks Plasma 6

Hello,

I'm facing very strange issues with STM32CubeIDE 2.0.0 under Linux Debian Trixie/Forky.
I'm running Kernel 6.17.11+deb14-amd64 with Plasma 6.5.4, KDE Framework 6.20.0 and QT version 6.9.2 in Wayland.

First issue is with debugger. I can start the firmware in debugging mode, runs but after few "Step Into" and "Step Over" commands the debugger is getting stuck. I doesn't take any commands anymore.

If I use "Restart" or "Terminate" or "Terminate and Relaunch" is starting again and again I can use few times "Step Into" and "Step Over"

 

Second issue is with windows ordering after using for a while STM32CubeIDE: it breaks completely the windows orders under Plasma and the only solution is to logout and login back and restart all apps.

I didn't get this issue with any other apps, except STM32CubeIDE.

2 replies

AScha.3
Super User
Dec 27, 2025 7:12 PM UTC

Hi,

i run LinuxMX , Debian system also, Xfce desktop, but i had no success with the Debian version, the generic version working.

Is still IDE 1.18.1 , and needed change to the GDB multiarch , the GDB didnt work (missing old libs).

 

So if you wanna try: install generic version...and check it.

If you feel a post has answered your question, please click on " Best Answer ".
EasyNet
EasyNetAuthor
Associate III
Jan 2, 2026 12:34 PM UTC

For me I was able to install the packages.

I'm using the CubeIDE GCC version 13 and 14. Both of them have the same behavior.

I will try to check if the OS GCC for ARM is working better.