Skip to main content
Associate
Nov 20, 2025 8:29 AM UTC
Solved

STM32CubeIDE 2.0.0 dark theme

v20.0.0_2.png

Hello,
It's been two years since version 1.14.1 (everything was fine there) – is it really that hard to remove these white scrollbars? It's impossible to use STM32CubeIDE...
BR

Ghofrane GSOURI
Ghofrane GSOURIBest answer
ST Technical Moderator
Nov 26, 2025 10:19 AM UTC

Hello @bobval @JensH @A.D. 

At present, STM32CubeIDE 2.0.0 is built on Eclipse Platform version 4.33.0.v20240903-0618 

The migration to a newer Eclipse version within STM32CubeIDE is planned for next year.

GhofraneGSOURI_0-1764151726472.png

The behavior reported by @bobval  is described in this LINK  

Additionally, the issue where Eclipse does not fully switch to "Dark Theme/Mode" is reported in the following LINK 

THX

Ghofrane

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

10 replies

Ghofrane GSOURI
ST Technical Moderator
Nov 20, 2025 10:48 AM UTC

Hello @bobval 

I tested this behavior using STM32CubeIDE 2.0.0 and did not encounter any white scrollbars.

Could you please let me know which operating system you are using?

GhofraneGSOURI_0-1763635594333.png

GhofraneGSOURI_1-1763635871584.png

 

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
bobvalAuthor
Associate
Nov 20, 2025 11:02 AM UTC

Windows 11 25h2 , (On Windows 10, everything was fine.)

Ghofrane GSOURI
ST Technical Moderator
Nov 20, 2025 11:20 AM UTC

Hello @bobval 

I performed the test on a Windows 11 machine and did not encounter this issue, which suggests that the problem may be specific to your environment.

GhofraneGSOURI_0-1763637150072.png

Let's try the following steps to troubleshoot:

1- Go to Settings > Personalization > Colors
2- Set "Choose your default app mode" to Dark.

GhofraneGSOURI_1-1763637636017.png

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
A.D.
Associate III
Nov 20, 2025 11:51 AM UTC

For those were darkmode currently works correctly:

Go to `Preferences -> General -> Appearance`. There, set `Color and font theme` to something different than the default and change it back. Do you still not have these big white scroll bars? For me they appeared after I changed some settings in the appearance dialog.

Associate II
Nov 26, 2025 7:52 AM UTC

Hi @Ghofrane GSOURI ,

I'm really sorry but I have the same problem with STM32CubeIDE2.0 and Windows 11 Pro 25H2. I have light grey scrollbars and can't even reproduce the dark ones.

My Windows color mode is dark, the IDE "Theme" is dark and the "Color and font theme" is Default (current). I have generated a new workspace with the IDE2.0 for testing and no addons are installed.

I have exported the settings that don't work.

 

Best regards,

Jens 

Ghofrane GSOURI
Ghofrane GSOURIBest answer
ST Technical Moderator
Nov 26, 2025 10:19 AM UTC

Hello @bobval @JensH @A.D. 

At present, STM32CubeIDE 2.0.0 is built on Eclipse Platform version 4.33.0.v20240903-0618 

The migration to a newer Eclipse version within STM32CubeIDE is planned for next year.

GhofraneGSOURI_0-1764151726472.png

The behavior reported by @bobval  is described in this LINK  

Additionally, the issue where Eclipse does not fully switch to "Dark Theme/Mode" is reported in the following LINK 

THX

Ghofrane

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
bobvalAuthor
Associate
Nov 26, 2025 2:59 PM UTC

Do you really have to wait until next year to find and replace two bytes from 0x00 to 0xFF in your own IDE?

 

Okay, thanks for the answer.