Skip to main content
March 24, 2022
Question

STM32CubeIDE 1.9.0 does not load EEPROM content when starting a debug session

As said in the title, if I have some EEPROM content in my source code, when starting the debugging session these data are not loaded, only the flash part is.

I must add that I'm talking about real EEPROM inside a STM32L010 device, not external EEPROM (which needs an external loader, that is OK) nor EEPROM emulation in flash (which will be loaded as part of the flash, that is OK).

Also why does the debugging session uses a temporary .srec file instead of the already generated .elf file that has already all the information in it (and CubeProgrammer can use without any problem) ?

Best regards,

Kraal

This topic has been closed for replies.

2 replies

TDK
March 24, 2022

What do you mean exactly? Do you want the EEPROM populated in the same way that the FLASH is populated when you program the chip? As in, it's a section within your linker script?

"If you feel a post has answered your question, please click ""Accept as Solution""."
KraalAuthor
March 24, 2022

Hi,

Yes, as in a section in my linker script

/* Specify the memory areas */
MEMORY
{
 FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 16K
 EEPROM (rx) : ORIGIN = 0x08080000, LENGTH = 128
 RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 2K
}
 
/* Further down in the script */
 .eeprom :
 {
 KEEP (*(.eeprom*))
 } >EEPROM

And in my C file

__attribute__((__section__(".eeprom"))) const uint16_t table[] = {/* here a table of values */};

As said, the generated ELF file has all the content in it.