STM32CubeIDE 1.8.0 Debugger starts, but exits immediately
I upgraded to 1.8.0 and it worked OK for a few days. Now whenever I try to Run or Debug (F11) program using ST-Link, the debugger starts, connects, but then immediately exits without error. The console shows:
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Shutting down...
Exit.The only hints are a directory called RemoteSystemsTempFiles showed up in my project root and I got a single line in the Problems window referring to a nature entry in my .project file. I'm a bit fuzzy on the last point, I cleared the error and it didn't return.
I've tried re-installing CubeIDE and restoring both the project root .settings directory. The issue does not appear to be project specific so not messed with project settings.
Hoping someone has some suggestions. Only thing I can think of next is going into the registry (Yes, Windows) and trying to delete anything STM32-related but that is really messy and dangerous.
Thanks in advance any suggestions.