Skip to main content
Markus GIRDLAND
ST Employee
Jul 26, 2021 9:01 AM UTC
Question

STM32CubeIDE 1.7.0 released

STM32CubeIDE 1.7.0 was released last week on st.com as well as an in-tool update patch.

Caution: The in-tool update does not allow updating debug probe drivers and ST-LINK server tool. Full installer is required for this.

What is new in 1.7.0?

  • Target support updated in-sync with STM32Cube ecosystem in general. In particular:
    • Added support for additional STM32U5 series devices.
  • Integration of STM32CubeMX 6.3.0, STM32CubeProgrammer 2.8.0.
  • Eclipse® update 2021-03 (Q1 release) with improved macOS® Big Sur support
  • Improved FreeRTOS and Azure RTOS ThreadX debug support : full call stack for all tasks in the Debug view.
  • Information Center updated with new Feature Highlight.
  • Project less debug support: debug is possible with an elf file and no STM32 project
  • Thread-safe malloc solution

Known issues fixed and problems and limitations

Please refer to the wiki.

Where do I obtain STM32CubeIDE 1.7.0?

Caution: After updating STM32CubeIDE, the post-update restart fails. STM32CubeIDE must be restarted manually.

This topic has been closed for replies.