Skip to main content
Associate III
Jan 9, 2026 11:02 AM UTC
Question

STM32Cubeide 1.19 and CubeMX 6.16 compatibility

Hello. 

My current set up is STM32Cubeide 1.19 which has an integrated version of the CubeMX (6.15)
I'm currently working on some st git examples, that seem to have been created with CubeMX (6.16), thus i cannot open the .ioc file on cubeIDE. I installed cubeMX 6.16 in order to edit the .ioc file and hit generate. 
Once i tried to build the project on cubeIDE though i got various errors

make: *** No rule to make target 'C:/Users/asantorinaios/STM32CubeIDE/workspace_1.19.0/BLE_Beacon/Drivers/STM32WBAxx_HAL_Driver/Src/stm32wbaxx_hal_gtzc.c', needed by 'Drivers/STM32WBAxx_HAL_Driver/stm32wbaxx_hal_gtzc.o'. Stop.
"make -j12 all" terminated with exit code 2. Build might be incomplete.

If i try to exclude said file from the build, i another similar error. 
Is the cubeMX 6.16 incompatible with the 1.19 cubeIDE. Do i need to download cubeide 2.0 or is there another solution ?

5 replies

Andrew Neil
Super User
Jan 9, 2026 11:20 AM UTC

If the examples were made with  CubeMX v6.16 then, presumably, they are intended for use with CubeIDE v2.0.0 ?

Note that you can install multiple versions of CubeIDE simultaneously (eg, both 1.19 and 2.0.0)  - you just need a separate Workspace for each.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Ghofrane GSOURI
ST Technical Moderator
Jan 9, 2026 12:03 PM UTC

Hello @AlexES 

You should be able to generate code with STM32CubeMX 6.16 and then open and build that project in STM32CubeIDE 1.19.

Could you please share your IOC in order to check your configuration .

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
AlexESAuthor
Associate III
Jan 9, 2026 12:29 PM UTC

I've inserted 2 .ioc files. the first is the one that i downlaoded from git with no MX editing and the second is after MX editing. I can successfuly build the first one, but not the second