Skip to main content
MHoll.2
Senior III
Jul 8, 2025 7:59 AM UTC
Solved

STM32CubeIDE 1.19.0 Problem migrating OCTOSPI2 (STM32H730) from 1.18.1

I have a ioc file created with Version 1.18.1, that enables only the OCTOSPI2 (and some RCC and clock settings).

Importing this file (see attachmend) the OCTOSPI2 gets disabled, further more it is non longer possibile to re-enable it as QUAD-SPI!

MHoll2_0-1751961259995.png

If added with out migration the IOC it is working as before.

MHoll.2
MHoll.2Best answer
Senior III
Nov 20, 2025 3:37 PM UTC

The problem seems to be resolved in STM32CubeMX 6.16.0 (together with STM32CubeIDE 2.0.2).

10 replies

ST Technical Moderator
Jul 8, 2025 8:40 AM UTC

Hello @MHoll.2 ,

 

First let me thank you for posting.

Your request is under investigation, and I will get back to you ASAP.

 

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ST Technical Moderator
Jul 8, 2025 12:33 PM UTC

Hello @MHoll.2 ,

 

Thank you for bringing this issue to our attention.

The issue is reported to the dedicated team under an internal ticket ( Ticket Number: 213708 ).

 

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Explorer
Jul 30, 2025 8:52 AM UTC

Hello, 

 

I've got the same issue here with an STM32H7A3. I need to enable the Quad configuration because otherwise proper codegen with FileX/LevelX will not work.

 

Any idea when it will be fixed?

 

MHoll.2
MHoll.2Author
Senior III
Jul 31, 2025 5:59 AM UTC

I decided to stay on the version 1.18.1 for the momento.

 

Associate
Aug 19, 2025 8:24 AM UTC

I am having the same issue with a fresh STM32H23VETx project (CubeMX 6.15.0):

screenshot.png

ST Technical Moderator
Aug 20, 2025 10:11 AM UTC

Hello @samdorey @MHoll.2 @Comet_SL9 ,

 

I will keep you informed when this issue is fixed.

 

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Visitor II
Sep 15, 2025 6:53 PM UTC

Hi @Mahmoud Ben Romdhane ,

Has this issue been resolved. I am trying to use the quadspi in my project.

Thanks

Andrew Neil
Super User
Sep 23, 2025 12:15 PM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
sigkukla
Visitor II
Nov 4, 2025 6:41 PM UTC

Also facing this issue with STM32CubeIDE 1.19.0 and am wondering if there's an update on this. I'd like to be able to use CubeMX code generation for this as opposed to manually configuring it. If not, did any of you find workarounds?

MHoll.2
MHoll.2AuthorBest answer
Senior III
Nov 20, 2025 3:37 PM UTC

The problem seems to be resolved in STM32CubeMX 6.16.0 (together with STM32CubeIDE 2.0.2).