Skip to main content
Associate II
Jan 19, 2026 10:21 AM UTC
Solved

STM32CubeIDE 1.19.0: GCC generates wrong code

I have a simple function with loop that checks RX pin state for 10ms, and if there was high level - breaks loop and exits. it works ok with -O0, but is broken with -Os or -O1 (-O2) or -Og - it loops forever.

Here's code:

uint8_t isModemOn() {
 uint32_t expire = uwTick + 10;
 while (expire - uwTick < 11) { // check RXD pin level, if low for 10ms - consider modem is off
 if (LL_GPIO_ReadInputPort(GPIOA) & LL_GPIO_PIN_10) {
 return 1;
 }
 }
 return 0;
}

and how it's appears in listing

080003dc <isModemOn>:
 * @PAram GPIOx GPIO Port
 * @retval Input data register value of port
 */
__STATIC_INLINE uint32_t LL_GPIO_ReadInputPort(GPIO_TypeDef *GPIOx)
{
 return (uint32_t)(READ_REG(GPIOx->IDR));
 80003dc:	21a0 	movs	r1, #160	@ 0xa0
//#pragma GCC optimize ("O0") // Error in -Os optimization

uint8_t isModemOn() {
 uint32_t expire = uwTick + 10;
 while (expire - uwTick < 11) { // check RXD pin level, if low for 10ms - consider modem is off
 if (LL_GPIO_ReadInputPort(GPIOA) & LL_GPIO_PIN_10) {
 80003de:	2380 	movs	r3, #128	@ 0x80
 80003e0:	05c9 	lsls	r1, r1, #23
 80003e2:	00db 	lsls	r3, r3, #3
 80003e4:	690a 	ldr	r2, [r1, #16]
 80003e6:	421a 	tst	r2, r3
 80003e8:	d0fc 	beq.n	80003e4 <isModemOn+0x8>
 return 1;
 }
 }
 return 0;
}
 80003ea:	2001 	movs	r0, #1
 80003ec:	4770 	bx	lr
	...

 I didn't work too much with ARM assembler, but  it looks like it calculates expire variable dynamically in the loop, or even dropped it's check at all. I tried to change conditions (while..if) but it doesn't help.

I'll try to find workaround by code refactoring, but I hope it'll be fixed in future releases.

NiTr0manBest answer
Associate II
Jan 19, 2026 10:52 AM UTC

Hm, I forgot to declare uwTick as volatile. with volatile all is OK...

2 replies

Andrew Neil
Super User
Jan 19, 2026 10:44 AM UTC

You haven't shown your definition of uwTick - is it the standard HAL one?

If not, is it volatile, and how is it updated ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
NiTr0manAuthorBest answer
Associate II
Jan 19, 2026 10:52 AM UTC

Hm, I forgot to declare uwTick as volatile. with volatile all is OK...