Skip to main content
DamageG
Associate II
May 4, 2024 9:04 PM UTC
Question

STM32CubeIDE 1.15.1 Not Generating Code

I have an STM32G474 project that has been working for some time but the latest update doesn't generate code from the .ioc config GUI.

If I make I make changes in the editor and select generate code, the pop flashes quickly and goes away but no code gets generated. I've tried this on a couple of Windows computers with the same result. 

This topic has been closed for replies.

3 replies

DamageG
DamageGAuthor
Associate II
May 5, 2024 1:45 PM UTC

I got it to work by starting a new project with the same processor. That gave me an error message that I didn't have the right firmware and needed to login and download. The requirement to be logged in is absolutely infuriating BTW.

After getting logged in and having the firmware download, the code would generate. But with an existing project, there was no error message that something was wrong. It would just pop up a window and close it without reporting any problem.

Rim LANDOLSI
ST Employee
May 7, 2024 2:58 PM UTC

Hello @DamageG  and welcome to the community,

Could you please check the connection and login to "myST" account to download the firmware and automatically generate the project

Hope this helps!

Thanks,
Rim

ASche.5
Associate III
Jul 28, 2025 6:48 AM UTC

This is a issue the code gen is just not done no msg or anything - also a newer CubeIDE.do this - @st_it at least let the user know that Cube has logged out for what ever... just cost me 20min to get that it has nothing to do with my project more with the customer tracking of ST. Do the tracking but don't f. up my UX for it please.