Skip to main content
Semer CHERNI
ST Employee
Mar 19, 2024 9:37 AM UTC
Question

STM32CubeIDE 1.15.0 released

STM32CubeIDE 1.15.0 was released today on st.com as well as an in-tool update patch.

  • What is new in 1.15.0?
    • Microcontroller and board lists aligned with STM32CubeMX v6.11.0 : STM32U0, STM32H7Rx/STM32H7Sx and STM32H523/STM32H533
    • Added the support for the Q-Format in the Live Expressions view
    • Added the support for Arm® Cortex®‑A7 registers in the SFRs view
    • Switched to GCC 12 as a default toolchain
    • Added the support for Fedora® 37 and macOS 14 (Sonoma)
    • Updated to Eclipse® 2023-12
  • Main fixed issues:
    • Refer to the STM32 microcontrollers wiki under this link.
  • Known issues fixed and problems and limitations:
    • Refer to the STM32 microcontrollers wiki under this link.
  • Where do I obtain STM32CubeIDE 1.15.0?
This topic has been closed for replies.

4 replies

PHolt.1
Senior
Mar 20, 2024 11:43 PM UTC

This new release has some problems:

https://www.eevblog.com/forum/microcontrollers/is-st-cube-ide-a-piece-of-buggy-***/msg5403485/#msg5403485

Well, this is hilarious. This forum software replaces the word c r a p with *** above, so you have to edit the URL manually!!!!

 

 

jhi
Senior
Mar 25, 2024 3:24 PM UTC

Do you even read the replies? Where can I write the bug report for the @-key not working on German-keyboard macOS because the *** ST-LOGIN is HARD CODED to ALT+L combo? It can't be so difficult to let the user change the key for that!

I have already wrote about this since version 1.13

Andrei Chichak
Lead
Apr 23, 2024 6:09 PM UTC

1.15.1 release notes please

Visitor II
May 15, 2024 2:18 PM UTC

Exception is thrown when trying to open .ioc file, created with the latest STM32CubeMX revision. This was not observed in previous version.
Exception:
This file has been generated with STM32CubeMX version '6.99.36'.Your current STM32CubeMX version is '6.11.1'.