Skip to main content
MSchm.1
Associate II
Feb 14, 2024 5:08 PM UTC
Question

STM32CubeIDE 1.14.1 Login to myST does nothing

With STM32CubeIDE 1.14.1 running on Windows10 the login to myST does not work anymore. Clicking the menu item or using the hotkey Alt-L simply does nothing - no reaction, no error message, NOTHING. It worked some time ago but all of a sudden does not work anymore. The Eclipse Log shows "Command 'com.st.stm32cube.ide.mcu.ide.command.userAuth.login' failed" if I try to login using myST.

Also the HELP menu items like "Manage Embedded Software packages" do nothing at all.

I tried to reinstall the software but the same result. My problem is now, that download of so far unsused processor support packages does not work, too.

Any idea?

This topic has been closed for replies.

17 replies

DBart.12
Visitor II
Dec 27, 2024 10:52 PM UTC

I have followed the manual to install Chromium:

https://docs.fedoraproject.org/en-US/quick-docs/installing-chromium-or-google-chrome-browsers/

After that I had to reboot my system (it didn't make any effect without it)

 

CubeIDE v1.16.1, Fedora 40 and all works fine.

Associate II
Feb 14, 2025 4:18 PM UTC

I am having the same problem withe CubeIDE 1.17.0. I cannot connect to MyST via Check For Updates or Manage Embedded Packages. There are a number of similar posts about this error, but I have not yet seen a definitive fix. My IT guy and I have over 8 hours on this issue! I checked Network Settings and Checked Connection worked. I installed Chrome and made it my default browser. I downloaded STM32Cube_FW_H7_V1.12.0 manually and pointed to it in CubeIDE. Still can't generate code. What is going on?