STM32CubeIDE 1.11.0 released
STM32CubeIDE 1.11.0 was released today on st.com as well as an in-tool update patch.
Caution: The in-tool update does not allow updating debug probe drivers and ST-LINK server tool. Full installer is required for this.
What is new in 1.11.0?
- Target support updated in-sync with STM32Cube ecosystem in general. In particular:
- Added the support for one new module in the STM32WL Series
- Added the support for one new board based on the STM32WB Series
- Added the support for one board based on the STM32F0 Series
- New video tutorials added in Information Center
- SEGGER J-Link update 7.82b
- Microprocessor Linux® bootloader deployment:
- Integration of OpenSTLinux Distribution v4.1.0
- Creation of “MPU SSH weston�? connection for GTK application debug
- SFRs view update
- Possibility to create tabs with subsets of peripherals and registers
- Dump of all peripheral registers to a file
- Possibility to read the registers via live channel
Additionally a new toolchain based on ST provided GCC-11 will soon be available as an in-tool patch update.
Known issues fixed and problems and limitations
Please refer to the wiki.
Where do I obtain STM32CubeIDE 1.11.0?
- https://www.st.com/stm32cubeide
- ... Or update your current installation of STM32CubeIDE using: Help > Check for updates
Caution: After updating STM32CubeIDE, the post-update restart fails. STM32CubeIDE must be restarted manually.