Question
STM32CubeF4 package versus the stm32cubeide package - what are the differences?
I intend to start a new project using the ST32F410, possibly first in a Nucleo package.
I have downloaded the STM32CubeF4 package as well as the stm32cubeide package.
What is the relationship between these two development packages offered by ST? Do I need them both, do they compliment each other, merge one into the other or are they seperate entities?
Where can I find example code for the ST32F410 in either of these packages?