Skip to main content
Associate
Oct 14, 2025 9:34 AM UTC
Question

STM32CubeCLT download option for macOS AArch64

On the download page for the STM32CubeCLT software, there is only a single download option available for macOS (STM32CubeCLT-Mac), which downloads the x86_64 version of the software.

Are there plans to add a download option for AArch64 macOS?

This topic has been closed for replies.

3 replies

Ghofrane GSOURI
ST Technical Moderator
Oct 14, 2025 10:49 AM UTC

Hello @liamclarkza 

From my understanding, the x86_64 version of the software is designed for Intel-based Macs and runs natively on those systems, providing optimal performance. On Apple Silicon Macs (which use the AArch64/ARM64 architecture), the x86_64 version can still be used thanks to Rosetta 2, a built-in translation layer that enables Intel-based applications to run seamlessly on Apple Silicon.

Therefore, the x86_64 version is compatible with both Intel and Apple Silicon Macs.

Are there any issues or limitations when running this version on Apple Silicon Macs (M1/M2) that we should be aware of?

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
Oct 14, 2025 11:27 AM UTC

Hi @Ghofrane GSOURI,

Thanks, yes, I have been using this through Rosetta currently with an Apple Silicon mac, but was hoping that there might be a download option for native aarch64. From what I have seen on the forums, it looked like there may have been an aarch64 version that was downloadable through the VSCode STM32CubeIDE plugin's bundle manager and so I was hoping this could be added as an option on the downloads page too. It would just be nice to have the native version instead of needing to download Rosetta and use an emulation layer if possible.

Ghofrane GSOURI
ST Technical Moderator
Oct 21, 2025 8:47 AM UTC

Hello @liamclarkza 

Your change request has been submitted to the development team under internal ticket number 220083.

I will keep you updated on any progress.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.