STM32Cube IDE on Fedora 37/38: .sh has outdated glib dependencies and Flatpak is problematic.
- 2 replies
- 2730 views
I am having difficulty getting STM32Cube IDE installed and running correctly on Fedora 37/38. The glib dependencies the .sh installer requires are outdated. I cannot list them because I moved on from that installation method days ago. I can get them if anyone thinks there is actually a chance of making it work.
The Flatpak installs, but there are issues with using something this complex from a Flatpak. I get an error about xdg-mime when trying to set external tools in settings, and nothing I could change in Flatseal would fix it. The problem is, as a beginner, I would not necessarily know if something was not working correctly if it seemed to compile, but some other problem was hiding. I have not received my board yet so I do not know if I will have problems connecting as I have read others have had.
My searches of The Google have lead me to dead ends when it comes to getting the IDE installed on Fedora. Has anyone had success on current Fedora releases using the .sh installer? Maybe someone has work around for using the Flatpak without issue? I wish Ubuntu would die. It is the Windows of Linux and everything is built to it. Worst case, I can install the IDE on Windows, but that is just a terrible thing to happen to anyone.
Edit: I have attached the log file from STM32CubeIDEVersion: 1.12.0 Build: 14980_20230301_1550 (UTC) Flatpak