Skip to main content
LWei.1
Associate
Oct 14, 2020 10:12 PM UTC
Solved

STM32Cube IDE 1.4.0 Device configuration tool deletes the project.

When I use .ioc file to generate the codes, it delete the entire project folder (include git information). Looks like I lose all the commits I haven't pushed to github. WTH is that.

This topic has been closed for replies.
TDK
TDKBest answer
Oct 14, 2020 11:31 PM UTC

There was an unfortunate bug in 1.4.0 that caused files to get deleted in certain cases. Might try updating to 1.4.2 to see if it's fixed.

"If you feel a post has answered your question, please click ""Accept as Solution""."

2 replies

TDK
TDKBest answer
Oct 14, 2020 11:31 PM UTC

There was an unfortunate bug in 1.4.0 that caused files to get deleted in certain cases. Might try updating to 1.4.2 to see if it's fixed.

"If you feel a post has answered your question, please click ""Accept as Solution""."
ST Technical Moderator
Oct 19, 2020 5:36 PM UTC

Hello @LW.2ei​ ,

This issue is fixed in the STM32CubeIDE v1.4.2, as mentionned in the STM32CubeIDE release note.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks