STM32 RCC Configuration with Register
Hi,
I am using STM32F407 discoveryboard and I am trying to set the RCC configuration such as the clock frequency is 168 MHz. I configure the register as I want but some bits at the RCC_PLLCFGR registers are already assigned to 1, and when I cleared these bits, the code wasn't work. I am adding the code below(I am using STM32CubeIDE) Could you help me please?
#define PLL_M 8
#define PLL_N 336
#define PLL_P 0 // PLLP = 2
extern uint32_t SystemCoreClock;
uint32_t systemClock;
void RCC_Config(void){
RCC->CR |= (1 << 16); // HSE On
while(!(RCC->CR & RCC_CR_HSERDY)); // Wait HSE Active
RCC->CR |= (1 << 19); // CSS On
RCC->PLLCFGR |= (1 << 22); // PLL Source is HSE
RCC->PLLCFGR |= (4 << 0); // PLL_M : 4
RCC->PLLCFGR |= (168 << 6); // PLL_N : 168
RCC->CR |= (1 << 24); // PLL is on
while(!(RCC->CR & (1 << 25))); // Wait PLL Ready
RCC->CFGR &= ~(1 << 0); // To set PLL, Bits(1:0) must be 10, so 0th bit is configured as 0
RCC->CFGR |= (1 << 1); // PLL selected as system clock
while(!(RCC->CFGR & (1 << 1))); // Select system clock is PLL
RCC->CIR |= RCC_CIR_HSERDYC;
RCC->CIR |= RCC_CIR_CSSC;
}
int main(void)
{
RCC_Config();
SystemCoreClockUpdate();
systemClock=SystemCoreClock;
while (1)
{
}
}