Skip to main content
August 19, 2020
Question

STM32 OTA? Goodbye to ST-Link? How to upload via internet?

I found a project that allows the programming of STM32 via OTA, it would be very interesting if the STM32CubeIDE could work directly with this.

[STM32 OTA using esp8266]:

https://www.youtube.com/watch?v=aqYHebO789U

Does anyone know if it is possible to use the STM32CubeIDE via OTA, just as it is already possible with the Arduino IDE?

I found another project with Raspberry Pi, maybe it can be adapted to work with the IDE directly:

https://github.com/disk91/PySWD

Example of use:

https://www.disk91.com/2015/technology/programming/swd-programming-using-a-raspberrypi/

This topic has been closed for replies.

2 replies

Piranha
Principal III
August 19, 2020

IDE and debugger are tools for development. OTA is a product feature allowing end-user to update firmware. User will not install IDE and OTA cannot debug - those are completely different things!

Tesla DeLorean
Guru
August 19, 2020

You know most of the recent DISCO/NUCLEO boards using the ST-LINK/v2-1 can act like mass-storage devices you can drag-n-drop binaries too.

Perhaps this could emulate a GDB Server?

This approach seems to add cost and complexity, where neither is needed. In most commercial applications debugging the device is a pretty fractional thing.

You know you can write your own IAP/OTA loaders into your boards now, and use whatever network or connectivity that already affords.

Plenty of people have implemented FOTA over WiFi, Cellular, etc using protocols like TFTP, FTP, HTTP, etc, where parts in the field have to auto-magically update, hopefully less frequently than Adobe Flash or Firefox, as that would likely blow the NB IoT data budgets..

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..