Skip to main content
Associate III
June 25, 2024
Question

stm32 modbus

I am working on stm32u0 with ultrasonic flow meter, i am facing an issue to receive the response from the device using Modbus communication

 

#include "main.h"
#include <stdio.h>
#include <string.h>
#include <stdint.h>
 
#define PUTCHAR_PROTOTYPE int __io_putchar(int ch)
#define GETCHAR_PROTOTYPE int __io_getchar(void)
#define MODBUS_SLAVE_ID 0x01
#define MODBUS_FUNCTION_READ_HOLDING_REGISTERS 0x03
uint8_t uart2_tx_data[8];
uint8_t uart2_rx_data[15];
uint16_t recv_data[2];
 
#define DATA_REGISTER_START_POSITIVE 115  // Positive accumulator value
#define DATA_REGISTER_START_NEGATIVE 117  // Negative accumulator value
#define DATA_REGISTER_START_NET      119  // Net accumulator value
 
int REGISTERS_TO_READ = 0x02;    // Number of registers to read
 
UART_HandleTypeDef hlpuart1;
UART_HandleTypeDef huart3;
 
PUTCHAR_PROTOTYPE
{
    HAL_UART_Transmit(&huart3, (uint8_t *)&ch, 1, HAL_MAX_DELAY);
    return ch;
}
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART3_UART_Init(void);
static void MX_LPUART1_UART_Init(void);
 
void modbusPreTransmission(void);
void modbusPostTransmission(void);
void sendModbusRequest(uint8_t *request, uint8_t len);
void ultrasonic_value(int DATA_REGISTER_START, int REGISTERS_TO_READ);
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart);
 
void modbus_tx_data()
{
 
    uint8_t slaveAddress = MODBUS_SLAVE_ID;
    uint8_t functionCode = MODBUS_FUNCTION_READ_HOLDING_REGISTERS;
    uint16_t startAddress = DATA_REGISTER_START_POSITIVE-1;
    uint8_t numRegistersHigh = 0x00;
    uint8_t numRegistersLow = REGISTERS_TO_READ;
 
    uart2_tx_data[0] = slaveAddress;
    uart2_tx_data[1] = functionCode;
    uart2_tx_data[2] = startAddress >> 8;
    uart2_tx_data[3] = startAddress & 0xFF;
    uart2_tx_data[4] = numRegistersHigh;
    uart2_tx_data[5] = numRegistersLow;
    uint16_t crc = crc16(uart2_tx_data, 6);
    uart2_tx_data[6] = crc & 0xFF;
    uart2_tx_data[7] = (crc >> 8) & 0xFF;
 
    printf("The Uart_tx buffer: ");
    for (int i = 0; i < 8; ++i)
    {
        printf("%02X ", uart2_tx_data[i]);
    }
    printf("\r\n");
 
    sendModbusRequest(uart2_tx_data, 8);
}
 
void modbusPreTransmission()
{
printf("Date pin enabled........\r\n");
    HAL_GPIO_WritePin(data_enable_GPIO_Port, data_enable_Pin, GPIO_PIN_SET);
    HAL_Delay(1000);
}
 
void modbusPostTransmission()
{
printf("Data pin disabled......\r\n");
    HAL_GPIO_WritePin(data_enable_GPIO_Port, data_enable_Pin, GPIO_PIN_RESET);
    HAL_Delay(1000);
}
 
void sendModbusRequest(uint8_t *request, uint8_t len)
{
    printf("Sending data to the Modbus...\r\n");
    modbusPreTransmission();
    if (HAL_UART_Transmit(&hlpuart1, request, len, 2000) == HAL_OK)
    {
        printf("\nSuccess : UART transmit done\r\n\n");
    }
    else
    {
        printf("\nError : UART transmit failed\r\n\n");
        return;
    }
 
    modbusPostTransmission();
 
    printf("Waiting for response...\r\n");
        HAL_Delay(100); // Adjust delay as necessary
 
        if (HAL_UART_Receive(&hlpuart1, uart2_rx_data, 7 + (2 * REGISTERS_TO_READ), 2000) == HAL_OK)
        {
            printf("Received data from Modbus: ");
            for (int i = 0; i < (7 + 2 * REGISTERS_TO_READ); ++i)
            {
                printf("%02X ", uart2_rx_data[i]);
            }
            printf("\r\n");
        }
        else
        {
            printf("Error: UART receive failed\r\n");
        }
}
 
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
    if (huart->Instance == LPUART1)
    {
        if (uart2_rx_data[1] == MODBUS_FUNCTION_READ_HOLDING_REGISTERS)
        {
            for (int i = 0; i < REGISTERS_TO_READ; i++)
            {
                recv_data[i] = (uart2_rx_data[3 + 2*i] << 8) | uart2_rx_data[4 + 2*i];
            }
 
            float data = *(float*)&recv_data;
 
            printf("Register Data: %f\r\n", data);
        }
        else
        {
            printf("Received unexpected data\r\n");
        }
    }
}
 
uint16_t crc16(uint16_t crc, uint8_t *data, uint32_t length)
{
  int i;
  crc ^= length;
  for (i = 0; i < 8; ++i)
  {
    if (crc & 1)
      crc = (crc >> 1) ^ 0xA001;
    else
      crc = (crc >> 1);
  }
  printf("The CRC : %x",crc);
 
  return crc;
}
int main(void)
{
  HAL_Init();
  SystemClock_Config();
  MX_GPIO_Init();
  MX_USART3_UART_Init();
  MX_LPUART1_UART_Init();
  printf("Welcome to stm32.......\r\n");
  HAL_Delay(2000);
  while (1)
  {
     modbus_tx_data();
HAL_Delay(5000);
  }
}
 
    This topic has been closed for replies.

    6 replies

    Andrew Neil
    Super User
    June 25, 2024

    Please see the posting guidelines - particularly how to properly post source code:

    https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228

     


    @sreedharan1196 wrote:

    I am working on stm32u0 with ultrasonic flow meter,


    Please give the full part number of the STM32, and details of the flow meter

     


    @sreedharan1196 wrote:

    i am facing an issue to receive the response from the device using Modbus communication


    What issue, exactly?

    What testing/investigation/debugging have you done to find the problem?

     

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Associate III
    June 25, 2024
    /* USER CODE BEGIN Header */
    /**
     ******************************************************************************
     * @file : main.c
     * @brief : Main program body
     ******************************************************************************
     * @attention
     *
     * Copyright (c) 2024 STMicroelectronics.
     * All rights reserved.
     *
     * This software is licensed under terms that can be found in the LICENSE file
     * in the root directory of this software component.
     * If no LICENSE file comes with this software, it is provided AS-IS.
     *
     ******************************************************************************
     */
    /* USER CODE END Header */
    /* Includes ------------------------------------------------------------------*/
    #include "main.h"
    
    /* Private includes ----------------------------------------------------------*/
    /* USER CODE BEGIN Includes */
    #include <stdio.h>
    #include <string.h>
    #include <stdint.h>
    
    #include "modbus_crc.h"
    
    /* USER CODE END Includes */
    
    /* Private typedef -----------------------------------------------------------*/
    /* USER CODE BEGIN PTD */
    
    #define PUTCHAR_PROTOTYPE int __io_putchar(int ch)
    #define GETCHAR_PROTOTYPE int __io_getchar(void)
    
    #define MODBUS_SLAVE_ID 0x01
    #define MODBUS_FUNCTION_READ_HOLDING_REGISTERS 0x03
    
    uint8_t uart2_tx_data[8];
    uint8_t uart2_rx_data[15];
    uint16_t recv_data[2];
    
    #define DATA_REGISTER_START_POSITIVE 115 // Positive accumulator value
    #define DATA_REGISTER_START_NEGATIVE 117 // Negative accumulator value
    #define DATA_REGISTER_START_NET 119 // Net accumulator value
    
    int REGISTERS_TO_READ = 0x02; // Number of registers to read
    
    /* USER CODE END PTD */
    
    /* Private define ------------------------------------------------------------*/
    /* USER CODE BEGIN PD */
    
    /* USER CODE END PD */
    
    /* Private macro -------------------------------------------------------------*/
    /* USER CODE BEGIN PM */
    
    
    /* USER CODE END PM */
    
    /* Private variables ---------------------------------------------------------*/
    
    UART_HandleTypeDef hlpuart1;
    UART_HandleTypeDef huart3;
    
    /* USER CODE BEGIN PV */
    
    PUTCHAR_PROTOTYPE
    {
     HAL_UART_Transmit(&huart3, (uint8_t *)&ch, 1, HAL_MAX_DELAY);
     return ch;
    }
    
    /* USER CODE END PV */
    
    /* Private function prototypes -----------------------------------------------*/
    void SystemClock_Config(void);
    static void MX_GPIO_Init(void);
    static void MX_USART3_UART_Init(void);
    static void MX_LPUART1_UART_Init(void);
    /* USER CODE BEGIN PFP */
    
    void modbusPreTransmission(void);
    void modbusPostTransmission(void);
    
    void sendModbusRequest(uint8_t *request, uint8_t len);
    void ultrasonic_value(int DATA_REGISTER_START, int REGISTERS_TO_READ);
    void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart);
    
    /* USER CODE END PFP */
    
    /* Private user code ---------------------------------------------------------*/
    /* USER CODE BEGIN 0 */
    
    void modbus_tx_data()
    {
    
    	 uint8_t slaveAddress = MODBUS_SLAVE_ID;
    	 uint8_t functionCode = MODBUS_FUNCTION_READ_HOLDING_REGISTERS;
    	 uint16_t startAddress = DATA_REGISTER_START_POSITIVE-1;
    	 uint8_t numRegistersHigh = 0x00;
    	 uint8_t numRegistersLow = REGISTERS_TO_READ;
    
    	 uart2_tx_data[0] = slaveAddress;
    	 uart2_tx_data[1] = functionCode;
    	 uart2_tx_data[2] = startAddress >> 8;
    	 uart2_tx_data[3] = startAddress & 0xFF;
    	 uart2_tx_data[4] = numRegistersHigh;
    	 uart2_tx_data[5] = numRegistersLow;
    //
    //	 uint8_t frame[] = {0x01, 0x03, 0x00, 0x72, 0x00, 0x02};
    //	 uint16_t len = sizeof(frame) / sizeof(frame[0]);
    //
    //	 uint16_t crc = crc16(frame, len-1);
    
    	 uint16_t crc = crc16(uart2_tx_data, 6);
    	 uart2_tx_data[6] = crc & 0xFF;
    	 uart2_tx_data[7] = (crc >> 8) & 0xFF;
    
    	 printf("The Uart_tx buffer: ");
    	 for (int i = 0; i < 8; ++i)
    	 {
    	 printf("%02X ", uart2_tx_data[i]);
    	 }
    	 printf("\r\n");
    
     sendModbusRequest(uart2_tx_data, 8);
    }
    
    void modbusPreTransmission()
    {
    	printf("Date pin enabled........\r\n");
     HAL_GPIO_WritePin(data_enable_GPIO_Port, data_enable_Pin, GPIO_PIN_SET);
     HAL_Delay(1000);
    }
    
    void modbusPostTransmission()
    {
    	printf("Data pin disabled......\r\n");
     HAL_GPIO_WritePin(data_enable_GPIO_Port, data_enable_Pin, GPIO_PIN_RESET);
     HAL_Delay(1000);
    }
    
    void sendModbusRequest(uint8_t *request, uint8_t len)
    {
     printf("Sending data to the Modbus...\r\n");
     modbusPreTransmission();
     if (HAL_UART_Transmit(&hlpuart1, request, len, 2000) == HAL_OK)
     {
     printf("\nSuccess : UART transmit done\r\n\n");
     }
     else
     {
     printf("\nError : UART transmit failed\r\n\n");
     return;
     }
    
     modbusPostTransmission();
    
     printf("Waiting for response...\r\n");
     HAL_Delay(100); // Adjust delay as necessary
    
     if (HAL_UART_Receive(&hlpuart1, uart2_rx_data, 7 + (2 * REGISTERS_TO_READ), 2000) == HAL_OK)
     {
     printf("Received data from Modbus: ");
     for (int i = 0; i < (7 + 2 * REGISTERS_TO_READ); ++i)
     {
     printf("%02X ", uart2_rx_data[i]);
     }
     printf("\r\n");
     }
     else
     {
     printf("Error: UART receive failed\r\n");
     }
    }
    
    void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
    {
     if (huart->Instance == LPUART1)
     {
     if (uart2_rx_data[1] == MODBUS_FUNCTION_READ_HOLDING_REGISTERS)
     {
     for (int i = 0; i < REGISTERS_TO_READ; i++)
     {
     recv_data[i] = (uart2_rx_data[3 + 2*i] << 8) | uart2_rx_data[4 + 2*i];
     }
    
     float data = *(float*)&recv_data;
    
     printf("Register Data: %f\r\n", data);
     }
     else
     {
     printf("Received unexpected data\r\n");
     }
     }
    }
    
    uint16_t crc16(uint16_t crc, uint8_t *data, uint32_t length)
    {
     int i;
     crc ^= length;
     for (i = 0; i < 8; ++i)
     {
     if (crc & 1)
     crc = (crc >> 1) ^ 0xA001;
     else
     crc = (crc >> 1);
     }
     printf("The CRC : %x",crc);
    
     return crc;
    }
    
    
    
    /* USER CODE END 0 */
    
    /**
     * @brief The application entry point.
     * @retval int
     */
    int main(void)
    {
    
     /* USER CODE BEGIN 1 */
    
     /* USER CODE END 1 */
    
     /* MCU Configuration--------------------------------------------------------*/
    
     /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
     HAL_Init();
    
     /* USER CODE BEGIN Init */
    
     /* USER CODE END Init */
    
     /* Configure the system clock */
     SystemClock_Config();
    
     /* USER CODE BEGIN SysInit */
    
     /* USER CODE END SysInit */
    
     /* Initialize all configured peripherals */
     MX_GPIO_Init();
     MX_USART3_UART_Init();
     MX_LPUART1_UART_Init();
     /* USER CODE BEGIN 2 */
    
     printf("Welcome to stm32.......\r\n");
     HAL_Delay(2000);
    
     /* USER CODE END 2 */
    
     /* Infinite loop */
     /* USER CODE BEGIN WHILE */
     while (1)
     {
     modbus_tx_data();
    	 HAL_Delay(5000);
     /* USER CODE END WHILE */
    
     /* USER CODE BEGIN 3 */
     }
     /* USER CODE END 3 */
    }
    
    /**
     * @brief System Clock Configuration
     * @retval None
     */
    void SystemClock_Config(void)
    {
     RCC_OscInitTypeDef RCC_OscInitStruct = {0};
     RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
    
     /** Configure the main internal regulator output voltage
     */
     HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE2);
    
     /** Initializes the RCC Oscillators according to the specified parameters
     * in the RCC_OscInitTypeDef structure.
     */
     RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI;
     RCC_OscInitStruct.MSIState = RCC_MSI_ON;
     RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT;
     RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_6;
     RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
     if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
     {
     Error_Handler();
     }
    
     /** Initializes the CPU, AHB and APB buses clocks
     */
     RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
     |RCC_CLOCKTYPE_PCLK1;
     RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_MSI;
     RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
     RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
    
     if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
     {
     Error_Handler();
     }
    }
    
    /**
     * @brief LPUART1 Initialization Function
     * @PAram None
     * @retval None
     */
    static void MX_LPUART1_UART_Init(void)
    {
    
     /* USER CODE BEGIN LPUART1_Init 0 */
    
     /* USER CODE END LPUART1_Init 0 */
    
     /* USER CODE BEGIN LPUART1_Init 1 */
    
     /* USER CODE END LPUART1_Init 1 */
     hlpuart1.Instance = LPUART1;
     hlpuart1.Init.BaudRate = 115200;
     hlpuart1.Init.WordLength = UART_WORDLENGTH_8B;
     hlpuart1.Init.StopBits = UART_STOPBITS_1;
     hlpuart1.Init.Parity = UART_PARITY_NONE;
     hlpuart1.Init.Mode = UART_MODE_TX_RX;
     hlpuart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
     hlpuart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
     hlpuart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
     if (HAL_RS485Ex_Init(&hlpuart1, UART_DE_POLARITY_HIGH, 0, 0) != HAL_OK)
     {
     Error_Handler();
     }
     if (HAL_UARTEx_SetTxFifoThreshold(&hlpuart1, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
     {
     Error_Handler();
     }
     if (HAL_UARTEx_SetRxFifoThreshold(&hlpuart1, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
     {
     Error_Handler();
     }
     if (HAL_UARTEx_DisableFifoMode(&hlpuart1) != HAL_OK)
     {
     Error_Handler();
     }
     /* USER CODE BEGIN LPUART1_Init 2 */
    
     /* USER CODE END LPUART1_Init 2 */
    
    }
    
    /**
     * @brief USART3 Initialization Function
     * @PAram None
     * @retval None
     */
    static void MX_USART3_UART_Init(void)
    {
    
     /* USER CODE BEGIN USART3_Init 0 */
    
     /* USER CODE END USART3_Init 0 */
    
     /* USER CODE BEGIN USART3_Init 1 */
    
     /* USER CODE END USART3_Init 1 */
     huart3.Instance = USART3;
     huart3.Init.BaudRate = 115200;
     huart3.Init.WordLength = UART_WORDLENGTH_8B;
     huart3.Init.StopBits = UART_STOPBITS_1;
     huart3.Init.Parity = UART_PARITY_NONE;
     huart3.Init.Mode = UART_MODE_TX_RX;
     huart3.Init.HwFlowCtl = UART_HWCONTROL_NONE;
     huart3.Init.OverSampling = UART_OVERSAMPLING_16;
     huart3.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
     huart3.Init.ClockPrescaler = UART_PRESCALER_DIV1;
     huart3.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
     if (HAL_UART_Init(&huart3) != HAL_OK)
     {
     Error_Handler();
     }
     if (HAL_UARTEx_SetTxFifoThreshold(&huart3, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
     {
     Error_Handler();
     }
     if (HAL_UARTEx_SetRxFifoThreshold(&huart3, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
     {
     Error_Handler();
     }
     if (HAL_UARTEx_DisableFifoMode(&huart3) != HAL_OK)
     {
     Error_Handler();
     }
     /* USER CODE BEGIN USART3_Init 2 */
    
     /* USER CODE END USART3_Init 2 */
    
    }
    
    /**
     * @brief GPIO Initialization Function
     * @PAram None
     * @retval None
     */
    static void MX_GPIO_Init(void)
    {
     GPIO_InitTypeDef GPIO_InitStruct = {0};
    /* USER CODE BEGIN MX_GPIO_Init_1 */
    /* USER CODE END MX_GPIO_Init_1 */
    
     /* GPIO Ports Clock Enable */
     __HAL_RCC_GPIOC_CLK_ENABLE();
     __HAL_RCC_GPIOA_CLK_ENABLE();
     __HAL_RCC_GPIOB_CLK_ENABLE();
    
     /*Configure GPIO pin Output Level */
     HAL_GPIO_WritePin(data_enable_GPIO_Port, data_enable_Pin, GPIO_PIN_RESET);
    
     /*Configure GPIO pin : data_enable_Pin */
     GPIO_InitStruct.Pin = data_enable_Pin;
     GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
     GPIO_InitStruct.Pull = GPIO_NOPULL;
     GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
     HAL_GPIO_Init(data_enable_GPIO_Port, &GPIO_InitStruct);
    
    /* USER CODE BEGIN MX_GPIO_Init_2 */
    /* USER CODE END MX_GPIO_Init_2 */
    }
    
    /* USER CODE BEGIN 4 */
    
    
    
    /* USER CODE END 4 */
    
    /**
     * @brief This function is executed in case of error occurrence.
     * @retval None
     */
    void Error_Handler(void)
    {
     /* USER CODE BEGIN Error_Handler_Debug */
     /* User can add his own implementation to report the HAL error return state */
     __disable_irq();
     while (1)
     {
     }
     /* USER CODE END Error_Handler_Debug */
    }
    
    #ifdef USE_FULL_ASSERT
    /**
     * @brief Reports the name of the source file and the source line number
     * where the assert_param error has occurred.
     * @PAram file: pointer to the source file name
     * @PAram line: assert_param error line source number
     * @retval None
     */
    void assert_failed(uint8_t *file, uint32_t line)
    {
     /* USER CODE BEGIN 6 */
     /* User can add his own implementation to report the file name and line number,
     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
     /* USER CODE END 6 */
    }
    #endif /* USE_FULL_ASSERT */
    Karl Yamashita
    Principal
    June 25, 2024

    You didn't enable UART interrupt so HAL_UART_RxCpltCallback will never be called. 

    If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
    Tesla DeLorean
    Guru
    June 25, 2024

    Not clear how the callback will occur here.

    Blindly waiting for a large block of data is probably not going to work.

    You have minimal control of the synchronization of received data, nor the ultimate length.

    You should perhaps recover a byte at a time, building a frame, getting it synchronized, and check CRC over the frame. Once you have a full valid frame, pass that on to another subroutine or process to decode / unpack.

    Do you have any colleagues or a supervisor who can work through the issues with you locally?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Associate III
    June 25, 2024

    will u plz guide me how to work with it 

    Pavel A.
    June 25, 2024

    Several Modbus projects are on github, have a look.

    https://github.com/urands/stModbus

    https://github.com/alejoseb/Modbus-STM32-HAL-FreeRTOS

    and more.