Skip to main content
Explorer II
May 7, 2025 1:45 PM UTC
Question

STM32-H755ZI system clock configuration error with changed CPU clocks from default

Hello everyone,

I choose the stm32 H755ZI (develop board) because I need a dual core microcontroller and a fast one. I never worked with dual core before (I did with STM32 and CubeIDE) so i let everything for default mode and tried to debug my project with this tutorial:

https://www.youtube.com/watch?v=jI1k6p-fduE&t=254s 

It worked and it seem time to change the settings too my project. 

My settings for the clock:

marte2003_0-1746624931635.png

RCC settings:

marte2003_1-1746625006429.png

 

and some other stuff with timers etc.

 

Then I wanted to debug again and the M4 core passed out and the M7 core ended up in this while loop in system clock config: 

marte2003_2-1746625077001.png

 

I tried multipel things: 1. lower clock config 2. lower clock config in combination with SMPS instead of LDO, but nothing works. Can anyone help me please? Thanks!!

 

Greetings from Holland 

 

 

 

This topic has been closed for replies.

1 reply

Semer CHERNI
ST Employee
May 14, 2025 4:04 PM UTC

Hello @marte2003 

First let me thank you for posting :) .

I need to ask what is the STM32CubeMX version used? The GUI seems to be the old one.

Also, the "SupplySource" generated code is not aligned with the STM32CubeMX configuration: In the STM32CubeMX the configuration is "PWR_SMPS_1V8_SUPPLIES_LDO" and in the generated code is "PWR_DIRECT_SMPS_SUPPLY"

KR,
Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.