Skip to main content
Associate
June 20, 2023
Question

STM32 GPIO state High After Earsing Microcontroller

  • June 20, 2023
  • 3 replies
  • 1090 views

Hello everyone,

I am using Stm32 controller for motor control and heating control. Universal motor is connected to TRIAC and TRIAC connected to MOC2023. LED of opto coupler is control by GPIO. Now problem is after erasing code from Flash memory , GPIO is high even though i have pull down resistor. At that moment , motor is still running  without code. What could be Approaches  that doesn't depended on Microcontroller ?

Thank you 

    This topic has been closed for replies.

    3 replies

    gbm
    Super User
    June 20, 2023

    You did not give any information that could allow anyone to help you. No MCU type, no pin identification

    Check the pin's default function, Maybe it's a JTAG pin. Maybe it's an UCPD DB pin.

    My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
    keyur1Author
    Associate
    June 20, 2023

    MCU is STM32G0B1RCT7 and pin is PB7

    gbm
    Super User
    June 20, 2023

    With Flash erased, the MCU enters boot mode automatically and maybe it sets the pin function for boot operation. Check the bootloader appnote for detailed info. PB7 is used as I2C pin in boot mode.

    My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice