Skip to main content
CTapp.1
Senior III
May 26, 2025 9:30 AM UTC
Solved

STLinkUpgrade utility text is too small to read

The font size used for the GUI in the STLinkUpgrade utility so small it is virtually unreadable on the external 32" 4K monitor that I use with my laptop. The following shows the text size relative to code within the IDE:

CTapp1_0-1748251211537.png

It's possible that this is as a result of using a 4K screen, as it looks ok when running on the laptop screen:

CTapp1_1-1748251544211.png

The size stays as above if I then close the lid, even though the external screen then switches back to 4K.

This topic has been closed for replies.
CTapp.1
CTapp.1Best answer
Senior III
May 26, 2025 3:52 PM UTC

It looks like setting the following properties on java.exe in STM32CubeIDE\plugins\com.st.stm32cube.ide.jre...\jre\bin helps:

CTapp1_1-1748274677672.png

Though the UI text is a lot fuzzier than the window title (the difference doesn't show that well in the above).

CTapp1_0-1748274581969.png

Still, I can now see what I'm doing ;)

All posts are made in a personal capacity. MISRA C++ Chair, MISRA C WG Member, Director The MISRA Consortium Limited (TMCL)

3 replies

Peter BENSCH
ST Technical Moderator
May 26, 2025 2:49 PM UTC

Which operating system are you using?

At least with Windows, this is not necessarily a problem with the application, but actually with Windows, which unfortunately has to be explicitly taught to use HR mode for every application.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
CTapp.1
CTapp.1Author
Senior III
May 26, 2025 3:25 PM UTC

This is Windows. How do I "teach it" what resolution to use? I don't recall it being a problem (with this application) in the past - though the "Start menu" is sometimes sharp and sometimes fuzzy (as if a low-resolution version has been upscaled badly).

I'm used to working with MacOS, so I've not run into this before!

All posts are made in a personal capacity. MISRA C++ Chair, MISRA C WG Member, Director The MISRA Consortium Limited (TMCL)
CTapp.1
CTapp.1AuthorBest answer
Senior III
May 26, 2025 3:52 PM UTC

It looks like setting the following properties on java.exe in STM32CubeIDE\plugins\com.st.stm32cube.ide.jre...\jre\bin helps:

CTapp1_1-1748274677672.png

Though the UI text is a lot fuzzier than the window title (the difference doesn't show that well in the above).

CTapp1_0-1748274581969.png

Still, I can now see what I'm doing ;)

All posts are made in a personal capacity. MISRA C++ Chair, MISRA C WG Member, Director The MISRA Consortium Limited (TMCL)