st-stm32cubeide_1.11.2_14494_20230119_0724.unsigned_amd64.deb_bundle.sh install issues
Trying to install on Windows 11 WSL2 Ubuntu 22.04.1 and get the following after accepting license:
Reading package lists... Done
Building dependency tree... Done
Reading state information... Done
Note, selecting 'st-stlink-server' instead of './st-stlink-server-2.1.0-1-linux-amd64.deb'
Note, selecting 'st-stlink-udev-rules' instead of './st-stlink-udev-rules-1.0.3-2-linux-all.deb'
Note, selecting 'st-stm32cubeide-1.11.2' instead of './st-stm32cubeide-1.11.2-14494-20230119-0724.unsigned_amd64.deb'
Note, selecting 'segger-jlink-udev-rules' instead of './segger-jlink-udev-rules-7.82b-linux-all.deb'
Some packages could not be installed. This may mean that you have
requested an impossible situation or if you are using the unstable
distribution that some required packages have not yet been created
or been moved out of Incoming.
The following information may help to resolve the situation:
The following packages have unmet dependencies:
st-stm32cubeide-1.11.2 : Depends: libncurses5 but it is not installable
Depends: libpython2.7 but it is not installable
E: Unable to correct problems, you have held broken packages.
Any ideas?