Skip to main content
Visitor II
January 17, 2024
Solved

ST-link v2 running on STM32Cube Programmer

I've recently bought a cheap Chinese ST-link v2 clone. It uses a Geehy APM32 MCU. Which is I guess  STM32 clone. I've since replaced it with a genuine STM32 MCU and st-link firmware. I was able to run it on  STM32 ST-link utility. But failed to run it on STM32CubeProgrammer. It wasn't detecting the st-link device. Is there a solution?

    This topic has been closed for replies.
    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    January 17, 2024

    Welcome @shovon134, to the community!

    As often discussed here in the community, clones are not accepted by the STM32CubeProg. Since there is no official binary of the original firmware, your ST-Link cannot be officially updated.

    Solution: get an original ST-LINK, either from a NUCLEO-64 or a genuine stand-alone ST-LINK. And forget these ST-LINK/V2 clones.

    Regards
    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    2 replies

    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    January 17, 2024

    Welcome @shovon134, to the community!

    As often discussed here in the community, clones are not accepted by the STM32CubeProg. Since there is no official binary of the original firmware, your ST-Link cannot be officially updated.

    Solution: get an original ST-LINK, either from a NUCLEO-64 or a genuine stand-alone ST-LINK. And forget these ST-LINK/V2 clones.

    Regards
    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    Tesla DeLorean
    Guru
    January 17, 2024

    >>Is there a solution?

    Buy legitimate / authentic equipment.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..