Some issues with STM32CubeIDE and STM32H747
1) In all of the examples the project explorer shows the CM7 code greyed and crossed out because "exclude from build" is checked. It is clearly not excluded from the build as this is the main code for the example. I presume this is some fiddle to allow eclipse to work with dual core processors but it is very confusing! Could you explain this?
2) In these examples main.h (and other include files) do not appear anywhere in the project explorer window yet they do exist and clearly used. What is going on here? If i need to view or edit the include files I need to resort to file manager.
3) For all of the examples you give project fies for IAR, Keil, and System Workbench but not for your own STM32CubeIDE. Why do you support third party tools and not your own?